2022-03-14 05:49 AM
I have attached a sample video, in which my desired work is being implemented.
implemented in the sample video.
As you can see the user can increase or decrease the text and can change the height and width at runtime as he wants.
Can we implement similar things in touch gfx ?
secondly, the user can add multiple texts in the box wherever he wants and return every parameter of the box x, y-axis, height, and width.
thirdly the box size is automatically resized according to the number of digits in it.
Kindly guide us, is nextion intelligent series is capable of doing these tasks?
2022-03-14 08:26 AM
Can we implement similar things in touch gfx ?
Maybe yes , but basic reply is TGFX dont have support for dynamic font size , then no.