2021-08-19 01:44 AM
I want to use graph drawing 2 line, in the MainView: : handleTickEvent () used in the graph. addDataPoint () to add data respectively?
Another requirement, line needs to be separated by some pixels, how to set.:face_with_tears_of_joy:
2021-08-19 06:14 PM
Line1 is the current effect, I want to achieve the effect of line2, the middle interval is wider
2021-08-19 10:00 PM
Sorry, but current version supports only continuous lines. That means you can't make breaks like you want. You can drop values down to -1 (or any other value below X axis) and keep it there for break period, but you will see vertical lines at the beginning and at the end of this "break"
2021-08-19 10:38 PM
Hopefully it can be improved in the future