cancel
Showing results for 
Search instead for 
Did you mean: 

How to propagate an event from the ModelListener to ALL presenters without the need to repeat the action in each presenter/viewer?

RMoha.2
Associate II

Examples presented show the declaration of an empty virtual method in the listener, and override it in the presenter.  However, in the case of multiple screens and the same action will be taken, there will be multiple redundancy.

15 REPLIES 15

Not that fast =) We're putting the final touches on 4.14.0 right now.

@Alexandre RENOUX​ What's the update regarding 4.14.0 release?

Hello,

I don't know exactly the day it will be out, but the 4.14 release is ready, it will be available along with the new version of CubeMX (6.0.0) by the end of next week normally.

/Alexandre

Is release 4.14 available?

Hi,

TouchGFX 4.14 is now available online with the release of CubeMX 6.0

/Romain

Hello,

Indeed the release 4.14 is available. You can get it on st.com or directly by updating to CubeMX 6.0.0 and get the new X-CUBE-TouchGFX-4.14 Package.

An official post on the Community will be posted soon.

/Alexandre