‎2021-11-08 1:32 PM
I have STM32H7A3ZIQ Nucleo board and 5" Startek LCD KD050FWFPA011. I'd like to use CubeIDE to create code to copy an image from H7A's flash memory to the LCD using LTDC. I did get STM32H7A3ZIQ Nucleo to work with a 2" LCD using 4-wire SPI interface. The problem I have with 5" LCD is the LTDC interface. Attached is IOC file, CubeIDE code, init code from Startek, scope captures, etc.... Please help.
I got black screen. Backlight is on. IDE reports the image (Mushroom480x800) is defined but not used. Scope captures show 0x00 on pin LTDC_R4. LTDC_CLK is 24MHz, correct as designed. What do I miss?
‎2021-11-08 2:17 PM
5" LCD spec.
‎2021-11-09 10:44 AM
For use LCD you need some step and condition meet. Show image is last step...
Try explain what is problem , is your lcd init accepted, can command to lcd show white lcd usw...
From Nucleo you need for RGB24 connect to LCD around 30 high speed signals ...
‎2021-11-09 11:37 AM
There are 3 areas problems could exist in: 1) LCD initializing, 2)wiring between nucleo board and LCD, and 3)configuring/using LTDC. I have double checked the 1st two areas and haven't found any problem. I'm still working with LCD manuf in those areas. For now, the area I need help the most from ST is the 3rd one (LTDC). So I would much appreciate if anyone could review the IOC and code to see if I miss anything (most likely), and provide detail instructions. I have read documents/sample code about LTDC I could find, but still couldn't get it to work.
Connection between nucleo and LCD is per the IOC file and attached schematics.
‎2021-11-09 12:14 PM
I'm able to send ALL_PIXELS_ON, ALL_PIXELS_OFF cmds to LCD repeatedly. LCD turns white and black repeatedly.
‎2021-11-09 12:25 PM
All except layer config seems good. LTDC layer is window onj display managed with memory framebuffer.
You in code need reserve memory and set it in Layer 0 - Color Frame Buffer Start Adress
When your config for layer is 565 then for example image 100x100 need 20000bytes .
I recomend start with internal memory and set 0 to 99 x and y ... Finaly this window is full LCD, but first step is simpler with small window.
Good is read LTDC appnote LCD-TFT display controller (LTDC) on STM32 MCUs - Application note
‎2021-11-09 1:33 PM
I already have memory reserve for Layer 0 - Color Frame Buffer Start Adress in MX_LTDC_Init() below:
static void MX_LTDC_Init(void)
{
/* USER CODE BEGIN LTDC_Init 0 */
/* USER CODE END LTDC_Init 0 */
LTDC_LayerCfgTypeDef pLayerCfg = {0};
/* USER CODE BEGIN LTDC_Init 1 */
/* USER CODE END LTDC_Init 1 */
hltdc.Instance = LTDC;
hltdc.Init.HSPolarity = LTDC_HSPOLARITY_AL;
hltdc.Init.VSPolarity = LTDC_VSPOLARITY_AL;
hltdc.Init.DEPolarity = LTDC_DEPOLARITY_AH;
hltdc.Init.PCPolarity = LTDC_PCPOLARITY_IPC;
hltdc.Init.HorizontalSync = 3;
hltdc.Init.VerticalSync = 3;
hltdc.Init.AccumulatedHBP = 33;
hltdc.Init.AccumulatedVBP = 33;
hltdc.Init.AccumulatedActiveW = 513;
hltdc.Init.AccumulatedActiveH = 833;
hltdc.Init.TotalWidth = 531;
hltdc.Init.TotalHeigh = 853;
hltdc.Init.Backcolor.Blue = 0;
hltdc.Init.Backcolor.Green = 127;
hltdc.Init.Backcolor.Red = 0;
if (HAL_LTDC_Init(&hltdc) != HAL_OK)
{
Error_Handler();
}
pLayerCfg.WindowX0 = 0;
pLayerCfg.WindowX1 = 480;
pLayerCfg.WindowY0 = 0;
pLayerCfg.WindowY1 = 800;
pLayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_RGB565;
pLayerCfg.Alpha = 0;
pLayerCfg.Alpha0 = 0;
pLayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_CA;
pLayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_CA;
pLayerCfg.FBStartAdress = 0;
pLayerCfg.ImageWidth = 380;
pLayerCfg.ImageHeight = 600;
pLayerCfg.Backcolor.Blue = 0;
pLayerCfg.Backcolor.Green = 0;
pLayerCfg.Backcolor.Red = 0;
if (HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN LTDC_Init 2 */
pLayerCfg.FBStartAdress = (uint32_t)Mushroom380x600;
/* USER CODE END LTDC_Init 2 */
}
I also tried a small image (Mushroom380x600). The result is the same.
‎2021-11-09 1:49 PM
From scope captures, I don't see data on RGB pins during active DE.
‎2021-11-09 10:10 PM
‎2021-11-10 7:30 AM
I tried below codes. It didn't help.
/* USER CODE BEGIN LTDC_Init 2 */
pLayerCfg.FBStartAdress = (uint32_t)Mushroom380x600;
if (HAL_LTDC_Init(&hltdc) != HAL_OK) Error_Handler();
/* USER CODE END LTDC_Init 2 */
--------and -------
/* USER CODE BEGIN LTDC_Init 2 */
pLayerCfg.FBStartAdress = (uint32_t)Mushroom380x600;
if (HAL_LTDC_Init(&hltdc) != HAL_OK) Error_Handler();
if (HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0) != HAL_OK) Error_Handler();
/* USER CODE END LTDC_Init 2 */
I also tried HAL_LTDC_DeInit(&hltdc) before HAL_LTDC_Init(&hltdc). It didn't help.