cancel
Showing results for 
Search instead for 
Did you mean: 

How to fix error 2?

Vlaty.1
Senior

Good afternoon. I made a working project on CubeIDE for a railway timetable (LWIP, FreeRTOS, DSI, HDMI). The project was created in the repository. But the management has a requirement to add a symbolic part (JPG or bmp image). There was a problem when docking the JPEG part to the project (Error 2). How do I remove the problem? With respect. Alexander

0693W00000AQ923QAD.png

This discussion is locked. Please start a new topic to ask your question.
16 REPLIES 16
Vlaty.1
Senior

Good afternoon. I created an empty project in CubeMX. LWIP, FreeRtos. After that, I added http. I send you the result with the project.0693W00000BZzLdQAL.png

Vlaty.1
Senior

Good afternoon. I created an empty project in CubeMX. LWIP, FreeRtos. After that, I added http. I send you the result with the project.

Vlaty.1
Senior

Good afternoon. I ran CubeMX version 6.0.1. I activated JPEG, FREERTOS, LIBJPEG,LWIP.

I started the code generation. Then I ran the compiler from CubeIDE. After that, there are no errors in the project.

Next, I activated the LWIP HTTP option in CubeMX. Then I started generating the code. Then I ran the

compiler again from CubeIDE. After that, I got error 2. Sincerely, Alexander.0693W00000BaERHQA3.png

So which part of "Please copy & paste the Console output as text" did you not understand?

So now I have to break out the image editor, and go through the forum's image upload palaver ...

0693W00000BaFczQAF.pngIt's telling you that it can't find any file called 'fsdata_custom.c'

So the obvious first question is: do you actually have an 'fsdata_custom.c' file anywhere in your project?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Vlaty.1
Senior

The 'fsdata_custom. c' file is present in the project.0693W00000BaFnsQAF.png

Vlaty.1
Senior

I found the cause of error 2 in my project. This is a random character in the path to the h folder. See the drawing. But why this error occurs when creating a standard project, I do not know.0693W00000BaG7iQAF.png

Vlaty.1
Senior

It is very important for me to know where the instructions are how to create a file of the type image_320x240_argb8888[76800] from my similar one?0693W00000BaHCtQAN.png