cancel
Showing results for 
Search instead for 
Did you mean: 

how to display the value in float using snprintf?

Angle
Associate II

Hi, how can i use the snprintf for float value in touchgfx? I want to display the data from the sensor in touchgfx lcd but in float

12 REPLIES 12

Have you checked if the "update" functions are called when needed and that the angle_pitch/... values are correct as well when debugging ? I would guess that those angle values are never updated if everything else is working fine on the screen.

/Romain

is okay I got it already

What do you mean ?