cancel
Showing results for 
Search instead for 
Did you mean: 

How to display superscript in feet cubic?

BParh.1
Senior III

I want to display the unit of volume as ft³. How can I do this in text widget of TouchGFX Designer?

1 ACCEPTED SOLUTION

Accepted Solutions

It probably also needs to be added to Wildcard Characters list in Typographies in the designer, otherwise it will display as ?

Embedded UI/UX Consulting: cadenza.design

View solution in original post

5 REPLIES 5
MM..1
Chief III

You try use Alt+0179 m³

It probably also needs to be added to Wildcard Characters list in Typographies in the designer, otherwise it will display as ?

Embedded UI/UX Consulting: cadenza.design
MM..1
Chief III

Too simply Ctrl C Ctrl V work, simple place it to Single use or Resource Texts size and font, then is added automatic, dont need list in Typogra...

You are correct, assuming they aren't going to use it in wildcards. Adding it to Typographies covers all use cases.

Embedded UI/UX Consulting: cadenza.design
BParh.1
Senior III

Thanks folks, so I just added '³' to Typography and copy paste the ft³ to my code, and it works as expected.