How set graphic on display with STM32 MCU?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-13 2:54 AM - edited ‎2023-11-20 8:17 AM
Hi,
I have this embedded display with resolution of 800x480, MIKROE-3620 which host at the back the STM32 MCU and many other features. I chose the STM32F746ZG as the MCU.
At first I created the project with MXCube, added TouchGFX component, build the project on Cube Ide, then I set the screen with TouchGFX and build it all with no error. The display is still black with no response. I also followed video, setted the SDRAM and QUADSPI, otherwise RAM and FLASH would overflow, but still no response.
With TouchGFX I just set 2 screens with button. A click on the button it would changes the screen.
So at this point, I have many doubts ...
I saw in many videos or documentation the use of LTCD periphery to control TFT display. Is it really necessary in my case, since the board has already a graphic driver? Here's the schematic of the display provided from the company. Even more, I'm afraid that when I activate LTDC, it selects pins that are assigned to others.
I also don't understand the communication protocol of the display. On the manual says that the touch control uses I2C communication, but I don't understand which communication protocol use the display?
I didn't plan to use FreeRTOS, but if it necessary is ok.
Here are some screenshot of SDRAM, QUADSPI and TouchGFX settings. I also uploaded the project.
What I'm doing wrong or I'm missing something?
- Labels:
-
LCD-LTDC
-
QSPI
-
STM32F7 Series
-
TouchGFX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-14 3:25 AM
Hello @stefyanna​ ,
I advise you:
- To start with an available example in STM32CubeF7: STM32Cube_FW_F7_V1.17.0\Projects\STM32746G-Discovery\Demonstrations\TouchGFX.
- To take a look at his MOOC.
I hope this help you!
Kaouthar.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-15 5:58 AM
I actually followed the same step and the display is still black...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-15 7:17 AM
Doesn't it use an SSD1963QL9 with 1.2M of internal frame buffer?
https://www.arrow.com/en/products/ssd1963ql9/solomon-systech
Examples from MikroE would be more appropriate than the STM32F746G-DISCO, which drives that screen from an SDRAM based frame buffer, and parallel RGB signals to the display. ie LTDC rastering data from local memory.
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
‎2023-04-15 12:12 PM - edited ‎2023-11-20 8:18 AM
Yes, exactly. It uses SSD1963 LCD display controller. In fact, as the picture shows:
The LCD_DATA[0-15] (marked with dotted res rectangle "GFX Sig)), WR#, RD#, D/C#, CS# (labelled in yellow) coincide with the pins of connector CN5 of the schematic.
I toook a look on the datasheet and still is not clear how to deal with the chip SSD1963. So far I understood, that I need to deal with a few pins, that are D[0:15], D/C#, CS#, RD#, WR#, RESET#, and TE, as the picture from the pdf shows:
But how? The datasheet a long command table and description, but I'm confused how to use it....
It also talk about a framebuffer, but how to set it and pass to TouchGFX and MCU STM32?
Any advice?