2019-04-06 3:42 AM
Hello,
I am currently trying to load a very simple TouchGFX (v 4.10.0) project to my STM32F469i-discovery (just a scene with a white background, a text and a button).
I created my project using CubeMX (v 5.1.0) and I was able to compile it, the screen just show the scene in the right way, but the problem is that the Touch Screen is not working.
So I noticed that the file:
{ProjectRoot}\TouchGFX\target\OTM8009TouchController.cpp
had some commented code, which I think i need to de-comment in order to let the Touch Screen works. The problem is that I need to include the BSP drivers which I have in an external folder on my computer:
C:\users\username\STM32Cube\Repository\STM32Cube_FW_F4_V1.24.0\Drivers\BSP\STM32469I-Discovery
I tried to add a "#include <stm32469i_discovery_ts.h>" after including the external folder into Project -> Build Settings -> C/C++ Build -> C Compiler -> Directories, but it continued to give me some errors (it could not found a reference to ft6x06_ts_drv at some point).
So, my question is: which is the correct way to include BSP Drivers into my project in order to let the touch screen work?
Thanks for your attention,
Mariano
Solved! Go to Solution.
2019-04-06 6:54 AM
Hi. Have you had a look at this post ... https://community.st.com/s/article/FAQ-Enable-touch-screen-on-the-STM32F746G-Discovery
2019-04-06 6:54 AM
Hi. Have you had a look at this post ... https://community.st.com/s/article/FAQ-Enable-touch-screen-on-the-STM32F746G-Discovery
2019-04-06 8:06 AM
Hi,
I followed step number 2 of that post and now everything is working fine! Here the files i had to include: stm32469i_discovery - lcd - sdram - ts
And also "ft6x06" from the folder Components
I finally had to resolve a conflict between two functions called in the same way, but they did the same things, so I commented one of the two and it worked for me!
Thank you!