Skip to main content
Krautermann
Senior
Jul 18, 2023 5:50 AM UTC
Solved

Honest opinion required: STemWin vs TouchGFX

I have to work on a long term project that involves using the LCD on the STM32H745XIH6 board and deciding which pathway to choose is crucial at the beginning of a project to avoid as much hassle as possible.

If I use STemWin, will I get support from the community here? If not, where can I get direct support? Does SEGGER still provide support for this?

Reason is, even though TouchGFX seems to be more user friendly in terms of modifying UI and creating amazing animation, I am not familiar with C++ and my boss seems unkeen to have a project mix with C and C++ due to difficulty in reading the assembly code when debugging errors. Plus we don't use RTOS and CMSIS in our project, so these have to be disable every time when creating project from TouchGFX.

This topic has been closed for replies.
Piranha
PiranhaBest answer
Principal III
Sep 6, 2023 3:00 PM UTC

The LVGL is under a MIT licence and therefore is free for virtually any use. What is not free is the related SquareLine Studio GUI editor, but that is not a mandatory tool.

8 replies

Joe WILLIAMS
ST Employee
Aug 10, 2023 6:10 PM UTC

Hello Krautermann

Your inquiry is being reviewed and our support team will be in touch with you shortly.

 

Kind Regards

Joe WILLIAMS

Piranha
Principal III
Aug 10, 2023 9:13 PM UTC

I'm not using any of these, but you should definitely take a look on LVGL.

https://www.reddit.com/r/embedded/comments/wfw4if/how_does_lvgl_compare_to_touchgfx_in_terms_of/

Krautermann
Senior
Sep 6, 2023 2:49 PM UTC

LVGL is nice because it's in C but the only problem is, it's not free if you want to use it for commercial use.

Piranha
PiranhaBest answer
Principal III
Sep 6, 2023 3:00 PM UTC

The LVGL is under a MIT licence and therefore is free for virtually any use. What is not free is the related SquareLine Studio GUI editor, but that is not a mandatory tool.

Pavel A.
Sep 10, 2023 2:12 PM UTC

Yes Segger continues to support (and sell) their emWin. Please visit their site and check the pricing options. They also have a public forum for emWin.