cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I have a question regarding Touchgfx.

Eakyo.1
Associate III

I want to drive 1.44 TFT with stm32f303 but flash is overflow. Can you help me? How about optimization touchgfx? In addition i dont use external flash. 

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
MM..1
Chief III

Memory ranges from 32 to 512 Kbytes and packages from 32 to 144 pins ???

Eakyo.1
Associate III

Memory is 256k but i can use 110k for touchgfx. Package from 48 pins. (stm32f303cct6)

MM..1
Chief III

This is edge, images set to L8 and optimization levels set to size

Even if I only describe it, it takes 70k flash. Only one empty box is defined. Optimization level is size