Senior III
April 9, 2022
Solved
STM32H7B3LI-DK (Tiny Shark) - Heap not initializing correctly; points to ITCM Ram 0x00000000
- April 9, 2022
- 5 replies
- 1934 views
Hi
Project built with TouchGFX not initializing heap properly:
When attempting to allocate a variable to the heap the variable is allocated at 0x00000000 instead of the heap location. This doesn't happen with projects built using cube. Does anyone have any ideas.
The screen shots are attached as my browser kept crashing when I tried to embed the images.
Project Built with CubeMX
Project built with touchGF, but with all TouchGFX code commented out and the MPU initialisation commented out as well:
I have asked this question on the support page.
The two projects are attached.
Best regards
Rob