2024-10-24 02:10 AM
Hello! First post on this forum.
I need to run automated testing of a TouchGFX application in an isolated environment.
The application takes screen snapshots and stores them to files.
It should not need a display to run if it can just render images to the display buffer and capture the result.
It runs on windows, and the framework I have uses docker containers, so it would be nice to
run headless, while still taking snapshots, in a windows build.
Is it possible to produce that kind of headless build? Would it run in a Windows Nano server container?
Best regards
/M