cancel
Showing results for 
Search instead for 
Did you mean: 

Has anyone been successful using STM MIPI-DSI with other then OTM8009A display driver? If yes which one?

ASmer.1
Associate II
 
2 REPLIES 2

Does the ADV7533 count?

ST7796H2 on IEG1120TB105GG-001 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
MM..1
Chief III

No. Item Specification Remark

1 LCD size 6.9 inch

2 Driver element a-Si TFT active matrix

3 Resolution 480(W) RGB x 1280(H)

4 Display mode Normally Black, Transmissive

5 Dot pitch 0.12546(w)x 0.12546(H)

6 Active area 60.22(W) x160.59(H) mm

7 Module size 66.50(W) ×180.80(H) ×4.7(D) mm Note 1

8 View direction ALL O’clock

9 Surface treatment Hard coating

10 Color arrangement RGB-stripe

11 Interface MIPI

12 Lcm power consumption ( 1.65W) TYP.

13 Drive IC NV3051D-T

MD069BL03-30IY-12A MIND