2024-03-09 09:55 AM
Requirments-
LCM->1024x600 TFT With CTP and Or 1028x 800 LVDS TFT With CTP
Color Depth-> 24bpp
FPS-> ~30
MCU-> _________?
RAM-> __________?
QSPI-> __________?
I have Selected the following Hardware But need expert opinion on this subject
My Selection-
MCU->STM32H750 BGA
SDRAM-> 16 BIT (IS42S32400F-6BL)QSPI->MT25QL512
The above parts are used in STM32H750B-DK
Solved! Go to Solution.
2024-03-14 04:08 AM - edited 2024-03-15 04:04 AM
Hello @ZExpo.1
As @MM..1 suggested, you should read the document to get more insight on why and what you need.
I'am adding some information on what @MM..1 suggested you :
I hope it helps,
Regards,
2024-03-09 10:40 PM
Hi try read an4861-lcdtft-display-controller-ltdc-on-stm32-mcus-stmicroelectronics.pdf
and self reply.
MCU without internal flash as 750 NO
SDRAM 16bit NO
QSPI any high speed
2024-03-14 04:08 AM - edited 2024-03-15 04:04 AM
Hello @ZExpo.1
As @MM..1 suggested, you should read the document to get more insight on why and what you need.
I'am adding some information on what @MM..1 suggested you :
I hope it helps,
Regards,
2024-03-14 09:51 AM
Thanks for the suggestions , As you specified in the 3rd bullet point that " In that case, you will either need a 32BITS SDRAM or a screen with embedded memory.
If you are using a complex GUI with a high-resolution screen, a MCU with internal flash is mandatory to store your framebuffer "
or You are saying I can use the Dual QSPI Setup as in STM32H750b-dk Board as external flash?
2024-03-14 10:11 AM
@LouisB make mistake in flash vs framebuffer. He mean high-resolutions screen require hign size graphics stored in flash (fonts images) . When your graphics is in internal flash bus overload go lower as for external QSPI.
2024-03-14 10:15 AM
I think the suggestion is that you really want 32-bit wide SDRAM to get adequate bandwidth, or internal SRAM, but it this case the size of the frame buffer would dictate where it can fit.
Suspect this is what Louis meant to say "MCU with internal SRAM flash is mandatory to store your framebuffer."
It might be able to pull static images from QSPI or DUAL-QSPI, but that's probably not a practical solution.
Some of the more specialized H7Ax and U599 devices had internal frame buffers, and resolutions / colour depths limited by that.
2024-03-15 04:06 AM
Internal RAM not flash, my bad.
2024-03-16 03:25 AM
So I got the following Calculation:-
Screen Resolution- 1280 x 800
Color Depth-24 Bpp
Framebuffer = (Resolution L * Resolution W * Color Depth)/8
=3,072,000 Bytes or 3.072 MB
For 1024 x600 TFT
Screen Resolution- 1024 x 600
Color Depth-24 Bpp
Framebuffer = (Resolution L * Resolution W * Color Depth)/8
=1,843,200 Bytes or 1.8432 MB
So what will be the calculation to get the FPS out from the system using CPU Frequency, RAM Bandwidth?
2024-03-16 04:15 AM
Simple math for example 60Hz == 3Mx60 one sec frames RAM trought 180MB/s (16 bit RAM 90MHz ...)
And calculations must be from oposite side you choice FPS and setup all clocks acord...
2025-02-06 05:41 AM
So to get 30 FPS at
Screen Resolution- 1024 x 600
Color Depth-24 Bpp
what system has to be implemented?