Hardware Selection for Advance HMI
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-09 9:55 AM
Requirments-
LCM->1024x600 TFT With CTP and Or 1028x 800 LVDS TFT With CTP
Color Depth-> 24bpp
FPS-> ~30
MCU-> _________?
RAM-> __________?
QSPI-> __________?
I have Selected the following Hardware But need expert opinion on this subject
My Selection-
MCU->STM32H750 BGA
SDRAM-> 16 BIT (IS42S32400F-6BL)QSPI->MT25QL512
The above parts are used in STM32H750B-DK
Solved! Go to Solution.
- Labels:
-
DMA2D (ChromArt)
-
TouchGFX
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-14 4:08 AM - edited ‎2024-03-15 4:04 AM
Hello @ZExpo.1
As @MM..1 suggested, you should read the document to get more insight on why and what you need.
I'am adding some information on what @MM..1 suggested you :
- Having a 1024*600 screen with 24bits with a lot of GUI/Animations, will engender a lot of memory transfers.
The bottleneck is the framebuffer access that will be done by the same bus for the LTDC and the graphic acceleration (ChromART/NeoChrom). - In that case, you will either need a 32BITS SDRAM or a screen with embedded memory.
If you are using a complex GUI with a high-resolution screen, a MCU with internalflashram is mandatory to store your framebuffer. - And a high speed QSPI is also needed with complex UI for a faster data transfer.
I hope it helps,
Regards,
ST Software Engineer | TouchGFX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-09 10:40 PM
Hi try read an4861-lcdtft-display-controller-ltdc-on-stm32-mcus-stmicroelectronics.pdf
and self reply.
MCU without internal flash as 750 NO
SDRAM 16bit NO
QSPI any high speed
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-14 4:08 AM - edited ‎2024-03-15 4:04 AM
Hello @ZExpo.1
As @MM..1 suggested, you should read the document to get more insight on why and what you need.
I'am adding some information on what @MM..1 suggested you :
- Having a 1024*600 screen with 24bits with a lot of GUI/Animations, will engender a lot of memory transfers.
The bottleneck is the framebuffer access that will be done by the same bus for the LTDC and the graphic acceleration (ChromART/NeoChrom). - In that case, you will either need a 32BITS SDRAM or a screen with embedded memory.
If you are using a complex GUI with a high-resolution screen, a MCU with internalflashram is mandatory to store your framebuffer. - And a high speed QSPI is also needed with complex UI for a faster data transfer.
I hope it helps,
Regards,
ST Software Engineer | TouchGFX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-14 9:51 AM
Thanks for the suggestions , As you specified in the 3rd bullet point that " In that case, you will either need a 32BITS SDRAM or a screen with embedded memory.
If you are using a complex GUI with a high-resolution screen, a MCU with internal flash is mandatory to store your framebuffer "
or You are saying I can use the Dual QSPI Setup as in STM32H750b-dk Board as external flash?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-14 10:11 AM
@LouisB make mistake in flash vs framebuffer. He mean high-resolutions screen require hign size graphics stored in flash (fonts images) . When your graphics is in internal flash bus overload go lower as for external QSPI.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-14 10:15 AM
I think the suggestion is that you really want 32-bit wide SDRAM to get adequate bandwidth, or internal SRAM, but it this case the size of the frame buffer would dictate where it can fit.
Suspect this is what Louis meant to say "MCU with internal SRAM flash is mandatory to store your framebuffer."
It might be able to pull static images from QSPI or DUAL-QSPI, but that's probably not a practical solution.
Some of the more specialized H7Ax and U599 devices had internal frame buffers, and resolutions / colour depths limited by that.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-15 4:06 AM
Internal RAM not flash, my bad.
ST Software Engineer | TouchGFX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-16 3:25 AM
So I got the following Calculation:-
Screen Resolution- 1280 x 800
Color Depth-24 Bpp
Framebuffer = (Resolution L * Resolution W * Color Depth)/8
=3,072,000 Bytes or 3.072 MB
For 1024 x600 TFT
Screen Resolution- 1024 x 600
Color Depth-24 Bpp
Framebuffer = (Resolution L * Resolution W * Color Depth)/8
=1,843,200 Bytes or 1.8432 MB
So what will be the calculation to get the FPS out from the system using CPU Frequency, RAM Bandwidth?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-16 4:15 AM
Simple math for example 60Hz == 3Mx60 one sec frames RAM trought 180MB/s (16 bit RAM 90MHz ...)
And calculations must be from oposite side you choice FPS and setup all clocks acord...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-06 5:41 AM
So to get 30 FPS at
Screen Resolution- 1024 x 600
Color Depth-24 Bpp
what system has to be implemented?