2022-02-08 5:56 PM
Hi,
I am using touchGFX version 4.16.1
setupScreenSAView::setupScreenSAView()
{
sliderHigh.setValue((uint16_t)((fanset_h1/2) * 10));
}
void setupScreenSAView::sliderMovedSAHigh(int value)
{
//report to presenter and update text
presenter->userSetSAFanSpeed();
}
A hardfault occurs when the above function is executed.
But
setupScreenSAView::setupScreenSAView()
{
//sliderHigh.setValue((uint16_t)((fanset_h1/2) * 10));
}
or
void setupScreenSAView::sliderMovedSAHigh(int value)
{
//report to presenter and update text
//presenter->userSetSAFanSpeed();
}
If I comment out sliderHigh.setValue(); or presenter->userSetSAFanSpeed(); the hardFault doesn't happen
I have to initialize the Slider and use the presenter as well.
How can I solve this problem ?
Best regards,
2022-02-10 2:04 AM
Hi,
Could you give a bit more context to your code and project ? Is the setupScreenSAView() function generated by TouchGFX Designer or is it a custom function (asking this because usually a screen setup would look like this: setup<screen name>View:: setupScreen() )? is the hardfault met in that setup function or in the slider moved function (what does that userSetSAFanSpeed() do exacly, meaning could the error come from it ?
Something to maybe try as well would be to create a variable (or const int) for the value you want to set instead of adding it in the function. It does help sometimes.
/Romain
2022-02-11 9:36 PM
Hi,
Thanks for the reply.
I changed it like you said and it works normally.
setupScreenSAView::setupScreenSAView()
{
//sliderHigh.setValue((uint16_t)((fanset_h1/2) * 10));
}
void setupScreenSAView::setupScreen()
{
setupScreenSAViewBase::setupScreen();
sliderHigh.setValue((uint16_t)((fanset_h1/2) * 10));
}
void setupScreenSAView::tearDownScreen()
{
setupScreenSAViewBase::tearDownScreen();
}
Best regards,