‎2020-04-18 05:13 AM
Hello,
I am developing an app using tortoise git, I have made a lot of commit and cleanup in rep and my application was ok.
Ten commits ago I never made a clean up, so, when I cleaned up the repository my app crash in one line of code I made before.
I am working with keil, I had clicked "generate code" in designer and then open keil and compile, but it crash in certain cases.
The app is working 70% before I cleaned up git it was 100%.
I really need urgent help.
Thanks
Solved! Go to Solution.
‎2020-04-21 05:30 AM
I think it is the JTAG ST-Link / V2 with an update it seems doesn't flash well using ST-Link Utility
I am flashing with another JTAG (same model V2) and it runs perfectly
:face_screaming_in_fear:
Thanks for your attention
‎2020-04-21 05:33 AM
Ouch!