2023-06-18 10:46 PM - edited 2023-06-19 12:14 AM
Hello friend!
Im working on TouchGFX GUI. Recently i have started learning thiis software using Diffrent diffrernt tutorials available online.
so i have configured FMC, I2C, Quad SPI, DMA2D and LTDC for STM32F746IGTx Controller according to the Data sheet of my touch Display.
After configuring every thing in CubeMx i added simple background and one Flex Button in TouchGFX and through that button im calling LED Blink function.
so when i done my actual coding and dumped the code into my controller its showing only my button and instead of background image its showing me a flicking background.
But im able to touch the button and through that LED is also getting toggeled.
i have uploaded my project files below. please check it and guid me how i should get GUI properly on Touch Display..?
FMC config:
QUADSPI:
DMA2D:
LTDC Parameters:
LTDC Layer:
TouhGFX settings:
CLOCK settings:
2023-07-09 11:52 PM
Thank you @uilter
i'll work on things that you have suggested me. i'll inform you whether it works or not.
Im using Open7xxi-c Board on that W25Q128JVSIM QSPI is there and link for its data sheet is:
https://pdf.tanssion.com/pdf/613/resource-files/w25q128jv-20revi-2008232021-20plus.pdf
and Im using FM24V10-G SDRAM and its data sheet link is :
https://pdf.tanssion.com/pdf/1/pdf/pcns/cypress-semiconductor/pin135228-part-marking.pdf
And Im using Wave share 7inch Touch Display and its data sheet link is:
https://www.waveshare.com/w/upload/1/1a/7inch_1024X600_LCD_DS.pdf
and when im taking TFT display frequency more 25Mhz im getting blank display, i have tried 32mhz and 40.8Mhz frequencies but if im using 25mhz and below 25mhz im getting flickring display as mentioned above.
2023-07-10 8:10 AM
Hi @JJhin.1 Let us know about this revision.
If you are using a dev board (Open7xxi-c Board) we can exclude for know any problem with the TFT power supply. But if possible, double check the values of VGH, VGL, AVDD and VCOM. These typ values are described in the LCD datasheet.
Thanks
2023-07-10 10:55 PM
These things are in 50 pin connector nah? im using 40 pin connector..
2023-07-11 2:34 AM - edited 2023-07-11 9:43 PM
i should also have to check 40 oin connector is properly connected to board or not..