STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! STM32H7S78-DK 1280x400 TFT

i'm referring to the STM32H7S78-DK which specifically mounts the new STM32H7S7L8 mcu there is the possibility of driving a 1280x400 rgb 888 or RGB 565 tft display using a double frame buffer with reasonable performance  we can carry out an example (F...

touch gfx display glitching

I`m currently using riverdi display RVT101HVSNWC00-B STM32 EMBEDDED 10.1" DISPLAY and im havinh a problem anything to my screen is glitching i tried images also gauges and texts am able to run the demos no problem but my screen always glitches the jo...

IMG_1264.jpg
ons by Associate
  • 1045 Views
  • 1 replies
  • 0 kudos

Resolved! How to make TouchGFX run on H747 M4 core

I am working with H747-DISCO (dual core) board and the issue is that I cannot choose the specific core which touchgfx runs on. It works well on M7 core but I need to use other software packs such as cube-ai on M7. So is it possible to manually switch...

Cizzy_Tim_0-1717588900422.png
Cizzy_Tim by Associate II
  • 2034 Views
  • 3 replies
  • 1 kudos

Resolved! scroll list inside scroll list

Hi,Currently I'm using touchgfx for designing screens for my Monochrome LCD (doesn't support Touch functionality). I'm using scroll list feature for displaying multiple items in one screen and use external button to scroll through them. Currently I s...

Enum.png
BhavyaSri by Associate III
  • 1415 Views
  • 1 replies
  • 2 kudos

Touchgfx; How to Play video from SD Card?

Hello everyone Is there any example that I can use to read avi file from SD- CARD and pass it to TouchGFX Function?Now I can play video from RAM at address 0xD0780000 for instance, This is TouchGFX Function but I don't know how to use it?Any help,  I...

Arisha by Associate II
  • 3428 Views
  • 5 replies
  • 2 kudos

Resolved! shared one Modal window for all screen

Suppose we have 50 different screen in a program.For the following modes, I have to show information to the user in a Modal window in the same screen we are in.For example, USB connection - correct storage of information in the memory - temperature c...

Natali by Associate III
  • 3353 Views
  • 5 replies
  • 1 kudos

Resolved! How to print on terminal while debugging TouchGFX

I'm using Visual Studio 2022 to develop and debug TouchGFX softwareEvery time I launch the debug the console output shows  'Application.exe' (Win32): download of 'C:\Windows\SysWOW64\windows.storage.dll' completed ... Thread 2792 exited with code 0 (...

nico23 by Senior III
  • 2067 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.