2024-11-19 05:40 AM
Hi,
I´ve to start a project (with FreeRTOS) where several code has to be implemented which is not directly related to the GUI (some state machines, control algorithms, ...).
I´m not sure, if I should implement this code parts as usual in my FreeRTOS and exchange only GUI data with the model, or if I should implement also my non GUI related code in the model?
Best regards,
Achim
2024-11-19 07:29 AM
Hello @AWack ,
Both would work.
You could include your main.h in the model.cpp to have access to the variables that are changed in main.c, this is straight forward and better for simple applications.
You could also use the RTOS if you have one which is great if you would need the semaphores / queue / other features of the RTOS so it is more suited for more complex applications.
Regards,