2019-09-17 11:28 PM
Im working on a STM32F407 MCU with an 320x240 px Display (16bit colors) connected to the FSMC. Id like to avoid using an external RAM.
Is it possible to have a smaller Framebuffer located in the internal RAM?
I guess it could be interesting to vary the buffer size to for example to 40 lines ( 320x40x16bit in my example) and putting the area to the internal RAM.
If its not possible might it be interesting to make a feature request?
Thank you in advance.
Solved! Go to Solution.
2019-09-18 03:40 AM
Not concretely. Internal deadlines are preventing us from releasing new versions, but this is being mitigated. Soon we'll have no restrictions on releasing new versions.
Hope that's enough of an answer!
/Martin
2019-09-17 11:56 PM
Hi @JB91,
Of course Just provide touchgfx with an address in internal memory instead of pointing to external RAM. Here's an example for how to configure touchgfx to use a single framebuffer in internal ram (most often, fitting two framebuffers in internal RAM is not feasible).
uint16_t frameBuffer[480 * 272];
static uint16_t frameBuf0 =&frameBuffer[0];
...
hal.setFrameBufferStartAddress((uint16_t*)frameBuf0, 16);
/Martin
2019-09-18 01:52 AM
Hi @Martin KJELDSEN ,
thanks for your quick answer.
Is it also possible to raster the framebuffer in order reduce the size of the framebuffer?
**example:**
With rastering it could be possible to split the framebuffer into several parts.
2019-09-18 02:14 AM
Hi @JB91,
In newer, yet to be released verisons of touchgfx, we support 8-bit palette and also partial framebuffers which both lower the overall memory requirements.
/Martin
2019-09-18 02:55 AM
Hi @Martin KJELDSEN ,
do you know when the new version will be released?
Thanks,
Josh
2019-09-18 03:40 AM
Not concretely. Internal deadlines are preventing us from releasing new versions, but this is being mitigated. Soon we'll have no restrictions on releasing new versions.
Hope that's enough of an answer!
/Martin