2024-05-06 3:21 AM
Hi,
The only way I can find to use a custom SVG as an Icon for a Flex Button is to add it to the Theme library.
As a workaround I created folder in the ..\designer\Themes\icon_theme\images\Themes directory and copied the SVG there. eg
C:\TouchGFX\4.23.2\designer\Themes\icon_theme\images\custom\example.svg
It seems to work ok but it is cumbersome. Is there a way to store the SVG with the projects assets or have I missed something?
Cheers,
Dan
2024-05-15 5:54 AM
Hello @codebuk ,
Thank you so much for pointing out this issue.
Yes, unfortunately, there is no simple way to add an SVG to a flex button from the project images. We will fix this issue as soon as possible.
Best regards,
2024-06-26 4:55 AM
Hello @codebuk ,
Sorry for the late response.
After discussing with the team, we have decided not to implement this feature for now. So, I suggest converting your SVGs to PNGs, or creating a custom container with an SVG and a flex button where the width and height of the flex button's Visual Element is set to zero.
Setting the visual element of the flex button to 0
I hope this helps!