cancel
Showing results for 
Search instead for 
Did you mean: 

Feature request: Ability to hide blue border in editor

Currently the blue border masks the pixels on the edge so you cannot see what you are doing.
Example:

unsigned_char_array_0-1743081297640.png

I want to be able to select and edit the widget while also seeing it completely.
I also want to be able to zoom in more than 500% and the ability to see a pixel grid. It's easy to be off by one.

(edit: removed section about scaling of the simulator window. Moved it to this topic: https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/feature-request-integer-scaling-for-simulator-rendering/m-p/788659#M42727)

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.
3 REPLIES 3
GaetanGodart
ST Employee

Hello @unsigned_char_array ,

 

Thank you for your feedback, I will inform the team about your request.

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

(I've moved this post about scaling to a new topic: https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/feature-request-integer-scaling-for-simulator-rendering/m-p/788659#M42727)

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.

very interesting, thanks