2023-02-24 2:21 AM
Hello,
I'm using stm32CubeIDE V1.9.
I wanted create new project example based on "LTDC_Display_1Layer".
Before - I deleted all folder related to this project (because I created it already and did something into but wanted start again from a fresh project) .
I also installed CubeIDE new.
Now I still get this stupid error, see screenshot below.
What can I do? New installation of V1.9 and new start of computer does not work...
Thank you
Solved! Go to Solution.
2023-02-24 3:15 AM
Hello @pk84
Do you mean you have deleted examples from the firmware package? If so, you need to redownload a new one or clone a repo from Github.
Try creating the project in a different location or directory to avoid conflicts and errors from the previous project.
Hope this helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-24 2:44 AM
I think, I've deleted the LTDC examples itself, where or how can I load it? (with other examples I can create a new project)
2023-02-24 2:53 AM
Hello @pk84 ?
You can refer to the CubeFW to find the LTDC examples.
Try to download the LTDC examples from Git or download a new FW from ST site .
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-24 3:15 AM
Hello @pk84
Do you mean you have deleted examples from the firmware package? If so, you need to redownload a new one or clone a repo from Github.
Try creating the project in a different location or directory to avoid conflicts and errors from the previous project.
Hope this helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-24 5:53 AM
I have deleted the whole folder and content in C:\Users\.....\STM32Cube\... so the IDE had to re-download everything, and now it works....
Of course, downloading the LTDC examples from Git would have been a solution too (I didn't know that these examples are available on Git...)
2024-08-16 3:51 AM
Seems this issue is still persisting even with the latest STM32Cube. I am having this same issue.
Does anyone know what the root cause is?
I have plenty of disk space in the folder used:
jannek@jannek-P720:~$ df -h .
Filesystem Size Used Avail Use% Mounted on
/dev/nvme1n1p1 916G 304G 567G 35% /home
jannek@jannek-P720:~$ uname -a
Linux jannek-P720 6.8.0-40-generic #40~22.04.3-Ubuntu SMP PREEMPT_DYNAMIC Tue Jul 30 17:30:19 UTC 2 x86_64 x86_64 x86_64 GNU/Linux
So, disk space should not cause any issues. The error note should also be more specific, now it's impossible to say WHAT file/package is the issue. 1st step would be to fix that, so one would have better means on debugging the root cause. This does not seem to create any sensible log lines to journalctl, either.