2020-10-07 5:22 PM
My company is currently in the process of developing a embedded UI and we had been hoping to use Emerging Display Technologies ETEML10100XDH6 board as it is has a pre built template by TouchGFX and can easily be flashed from the designer.
We were sent the ETEMB101008XDRAM instead, due to supply and price, which is almost identical barring the use of a STM32H7 vs the STM32F7 on the ETEML. Is there any plan to provide a prebuilt template for the ETEMB or will I need to follow the process of flashing a custom board due to the differing MCU's or is there something I can do with my current designer project, such as building the binaries and flashing using ST-LINK?
Solved! Go to Solution.
2020-10-29 8:37 PM
send a mail to support@edt-europe.com and we will provide the application template for ETEMB101008XDRAM for Designer V4.15.0 to you.
/Paul
2020-10-07 7:12 PM
Hello,
This is not something that TouchGFX can answer as we do not develop those boards. Try to ask EDT for that.
/Alexandre
2020-10-23 4:30 AM
Hi LIver.1 ,
Just of curiosity did you get what you needed ?
2020-10-29 8:37 PM
send a mail to support@edt-europe.com and we will provide the application template for ETEMB101008XDRAM for Designer V4.15.0 to you.
/Paul
2020-11-06 10:36 AM
Yes after reaching out to the company directly they supplied me with the template necessary.