2021-12-30 05:56 AM
After a good starting download stall ...
Either with firefox or google under ubuntu 20, it is the touchGFX designer 450Mo.
Regards.
JP
Solved! Go to Solution.
2021-12-31 11:54 AM
https://drive.google.com/file/d/1oq7sNL2olyw5PsFTgg31HheEcQE8S5Hv/view?usp=sharing
2021-12-30 11:50 AM
ST has had server/cache issues in the past, but typically has 2 or 3 delivery methods. Choose the email method if the direct download method fails.
2021-12-31 02:16 AM
Hi,
How to change the way to download ?
By email i wont be allowed to have such big attached document.
Is there a torrent file ?
JP
2021-12-31 06:01 AM
They email a link serviced by a different server.
No, torrents have been suggested before as a means of reducing server load and speed of download, and also the ability to recover/restart where service is slow, poor or intermittent.
Things can also be mirrored.
2021-12-31 11:54 AM
https://drive.google.com/file/d/1oq7sNL2olyw5PsFTgg31HheEcQE8S5Hv/view?usp=sharing
2022-01-02 12:58 AM
Hi,
Thanks for that link, it has loaded the file quite rapidly.
Installed in CUBEIDE, but the TouchGFXDesigner msi file doesnot install. I am with ubuntu 20 and wine launch correctly the msi, accept the license, choose shortcut and install path (let default wich not contain space) and appear an info box "Path cannot contain spaces" and that stop the installation.
I think the "space" are in the repertory name installed by the msi.
In anyway i thank you for the link, so i have the SDK, i think the msi install a GUI and i can do app with the sdk.
Regards
JP