2019-07-05 8:13 AM
Currently TouchGFX generates code (my target is a STM32F469 DISCOVERY board) that is based on the ST CubeMX framework. Is the 'mbed' framework on the roadmap, since I like it *a lot* better.
Solved! Go to Solution.
2019-07-09 5:39 AM
Hi @AMege,
TouchGFX does not directly support any framework. It is an independent framework and rendering mechanism. CubeMX helps configure projects so that what is required for TouchGFX to run (memory, LTDC, display, etc) are available.
Does that answer your question?
Best regards,
Martin
2019-07-09 5:39 AM
Hi @AMege,
TouchGFX does not directly support any framework. It is an independent framework and rendering mechanism. CubeMX helps configure projects so that what is required for TouchGFX to run (memory, LTDC, display, etc) are available.
Does that answer your question?
Best regards,
Martin
2019-07-09 8:47 AM
To be more precise:
What you would do is use the mbed framework to do what you want and then maybe present some data in your TouchGFX application. Check https://community.st.com/s/question/0D50X0000AU4zodSQB/interfacing-with-hardware-in-touchgfx-applications for inspiration on how to interface with hardware and generally present data coming from other tasks.
/Martin
2019-07-09 9:14 AM
Hi Martin,
thank you for your response, however I fail to understand how the generated code from TouchGFX, heavily using the CubeMX HAL layer to access the board resources can be replaced with the mbed HAL layer??
I already know how to interface with hardware in a TouchGFX application (both ways), but that was based on a project that did not use the mbed framework.
The mbed framework is a much higher level API than the ST CubeMX HAL drivers (that I don't like very much).
Regards,
/Antoine
2019-07-10 12:09 AM
Hi Antoine,
What i'm trying to say is that TouchGFX does not really care about which HAL you're using. It only requires some memory to render frames into and that you've set up whatever display interface you're using to transfer the pixels rendered to that buffer to the display. That's why you can take a TouchGFX GUI and run it on SDL2 simulator and on any hardware configuration that matches the dimensions of the application.
/Martin
2019-07-10 2:34 AM
I understand, but I don't know how to "strip" the CubeMX generated code from the TouchGFX project and replace it with the mbed HAL layer.
Are there howtos for this?
2019-07-10 2:42 AM
I guess there aren't any .. yet :) Do you really need CubeMX in this case? Anything you configure will be configured using STs HAL. If you start from one of the application templates from inside the designer i think this will become more apparent to you. Look into BoardConfiguration.cpp.
Let me know!
/Martin
2019-07-10 2:43 AM
In other words, when I click the "Generate Code" button, how can I control what HAL layer is used?
2019-07-10 3:05 AM
"Do you really need CubeMX in this case?"
No, I don't
"Look into BoardConfiguration.cpp."
Ok, but this is generated code, how can I control the generation process so it produces a different BoardConfiguration.cpp?
Or do I need to "hack" this file and every time I use "Generate Code" loose my changes?
2019-07-10 3:54 AM
BoardConfiguration.cpp is not generated code. It's a part of the port for the particular board when coming from our application templates.
/Martin