2018-11-22 08:14 PM
I upgraded my CubeMX to 5.0.0 and installed F4 1.22.0 firmware recently.
So, I tried to use CubeMX build a TouchGFX Project that use TrueSTUDIO as IDE.Since I was successful run a STemWin Project as my custom F429IGx board graphic solution.
In order to enable TouchGFX middleware in CubeMX, I activated and configured FreeRTOS, CRC, LTDC, DMA2D, TIM7 and FMC-SDRAM1.All setting were the same with my previous STemWin project, excepted in GRAPHICS I used TouchGFX as Graphics Framework. And then I generated code.
1. When opened the project, there were *.c , *.cpp , *.h and *.hpp files. But in C/C++ Build - Tool Setting , neither C++ Compiler and C++ Linker existed. So if I build the project under this settings, I will get a link error say something like main function undefined. Because main function is in main.cpp file and wound't be compile by GCC like other cpp files.
2. So I converted the project to C++ project, by using File - New - Convert to a C/C++ Project (Adds C/C++ nature) method. Now the C++ Compiler showed up and C++ Linker replaced C Linker.I built the project again, but a ton of error message like head files couldn't find show up. I fixed by copied and changed include path from C compiler directories to C++ compiler.But things not go well,some directories in Project Resources Manager's Includes still in grey which implicate those directories did not exist in that location.
3. Then I use TouchGFX Designer to generated a simple project which is only contains a single screen of a text and a background image.After code generation, I put the entire folder in TrueSTUDIO project's root. Now the "Includes" didn't has grey directories any more.I dragged all the cpp files which is generated by TouchGFX Designer into TrueSTUDIO project path [Application-User-TouchGFX-generated|gui].Things going in here is a bit out of my ability, since I am new in TouchGFX and new in mixin C(GCC) and C++(G++) code together.
4. I tried out lots of combination of Assembler, C Complier, C++ Complier, C++ Linker settings which mention in TouchGFX website.I can't describe all of them.The best result I can get is all c files compile into *.o successfully by GCC and all C++ files compile into *.o successfully by G++, but when executed
arm-atollic-eabi-g++ -o LC-MC001.elf *.o ...
command,which as we know is linking, tons of error show up.
d:/program files (x86)/atollic/truestudio for stm32 9.0.0/armtools/bin/../lib/gcc/arm-atollic-eabi/6.3.1/../../../../arm-atollic-eabi/bin/ld.exe: error: LC-MC001.elf uses VFP register arguments, Application\User\Core\main.o does not
d:/program files (x86)/atollic/truestudio for stm32 9.0.0/armtools/bin/../lib/gcc/arm-atollic-eabi/6.3.1/../../../../arm-atollic-eabi/bin/ld.exe: failed to merge target specific data of file Application\User\Core\main.o
d:/program files (x86)/atollic/truestudio for stm32 9.0.0/armtools/bin/../lib/gcc/arm-atollic-eabi/6.3.1/../../../../arm-atollic-eabi/bin/ld.exe: error: LC-MC001.elf uses VFP register arguments, Application\User\TouchGFX\generated\ApplicationFontProvider.o does not
d:/program files (x86)/atollic/truestudio for stm32 9.0.0/armtools/bin/../lib/gcc/arm-atollic-eabi/6.3.1/../../../../arm-atollic-eabi/bin/ld.exe: failed to merge target specific data of file Application\User\TouchGFX\generated\ApplicationFontProvider.o
...
5. The last information about this I can find is related to floating point implementation? I already tried to switch all implementation to HW or SW the same time.But no luck.
UPDATE
6. I switch Assembler, C compiler, C++ compiler, C++ Linker floating point option to Hardware implementation.And remove -mfloat-abi=softfp parameter which is recommend by this article:
https://touchgfx.zendesk.com/hc/en-us/articles/206116381-Using-other-IDEs-with-TouchGFX
So, after that, all of the processor will have a united floating point setting. Then put SysTick_Handler function back into stm32f4xx_it.c file. Finally, my project build without any error for the first time.
7. I download the program in my board. Sadly, I got this.
And my original design is below.
I will keep you update if any further information.
Thanks for your reading, I know it's a very long problem description.😂
Solved! Go to Solution.
2018-12-05 05:16 AM
Hi @Zhi Pang ,
After some investigations, it seems that there are some generation problems when using TrueStudio and TouchGFX.
I advice to switch to SW4STM32 until this issue is fixed.
We are sorry for the disturbance this issue may bring.
2018-12-05 09:28 AM
I just tried to build a TouchGFX project for STM32F746-DISCO using SW4STM32. I followed the instructions of the tutorial as best as I could. I created a new simple GUI rather than importing an older TouchGFX GUI. Unfortunately it didn't build either.
I encountered the following error: C:/Users/Administrator/workspace/SW4STM32_TouchGFX_Test/Middlewares/ST/TouchGFX/touchgfx/framework/include/platform/hal/simulator/sdl2/HALSDL2.hpp:22:10: fatal error: SDL2/SDL_video.h: No such file or directory
#include <SDL2/SDL_video.h>
I have attached my project file. Please let me know if I made and error in creating the project.
2018-12-06 12:08 AM
Hi @Clark Sann
This is a GCC IDE constraint that doesn't accept long paths.
Try to get a shorter path for your project
As a test you can replace the "SDL2" folder under your include generated by STM32CubeMX
2018-12-06 01:21 PM
@Nawres GHARBI
The path to the missing file (SDL2/SDL_video.h) is C:\Users\Administrator\workspace\Test\Middlewares\ST\TouchGFX\touchgfx\framework\include\platform\hal\simulator\sdl2\vendor\SDL2
That path is only 128 bytes. Isn't the windows limit 260 bytes?
I think the problem is that CubeMX did not put the correct include paths into the SW4STM32 project. When I add the above path to the list of include paths, the compiler is able to find the missing file.
However it still doesn't build because it then can't find <shellapi.h>. I can't fix this since this file is not included by CubeMX.
2018-12-07 04:39 AM
Hi @Clark Sann
I moved all the SDL folder under include folder generated by STM32CubeMX and it compiles ok, How did you from your side.
For the Shellapi.h, as you generated an under root project all the files have been added to the project even if not needed.
Shellapi.h stands for a library used by windows to build interfaces on the simulator.
To avoid this issue please remove all the simulator generated files from the projects
2018-12-07 10:45 AM
@Nawres GHARBI
I don't think the problem is with a long path. I was able to include the SDL2 folder by adding this path
"Middlewares/ST/TouchGFX/touchgfx/framework/include/platform/hal/simulator/sdl2/vendor/"
to the Project Properties -> C/C++ General -> Paths and Symbols. This keeps me from having to change the Middlewares/St/TouchGFX path structure.
I then deleted MyProject/TouchGFX/simulator. I found I could not delete other simulator folders located in Middleware/ST/TouchGFX because those files were needed for compilation of other non-simulator related files.
When I build now I get a LOT of errors. I will include my project.
Since you are able to get a project to build by relocating the SDL (or did you mean SDL2 folder?), please provide me more details on what you did. And also please tell me exactly what simulator generated files you deleted.
Thank you Nawres for your help. I feel I am close to being able to build my TouchGFX project. I have been trying to get it done for months.
2018-12-08 10:20 PM
I have same issues with project generated by CubeMX 5.0 for STM32F746 discovery board. IAR project compiles just fine, but TrueStudio's isn't.
Once I'm adding TouchGfx into project, project must be manually converted from C to C++, all sorts of undefined symbols and simulator code which I think should be excluded from build. After few days of kung fu with TrueStudio, I gave up.
2018-12-08 10:46 PM
on the other hand, STM32 Workbench project compiled almost out of box: I had to manually exclude source files for simulator from compilation:
Middlewares\ST\TouchGFX\touchgfx\framework\source\platform\hal\simulator\sdl2\*.cpp
TouchGFX\simulator\*.*
2018-12-09 10:21 AM
@PPiar
For some reason, when I do what you suggested, I still cannot build. Here is exactly what I am doing:
Building file: ../Middlewares/ST/TouchGFX/touchgfx/framework/source/platform/driver/touch/SDL2TouchController.cpp
Invoking: MCU G++ Compiler
C:\Users\Administrator\workspace\Test_SW4STM33\Debug
arm-none-eabi-g++ -mcpu=cortex-m7 -mthumb -mfloat-abi=hard -mfpu=fpv5-sp-d16 '-D__weak=__attribute__((weak))' '-D__packed=__attribute__((__packed__))' -DUSE_HAL_DRIVER -DSTM32F746xx '-DUSE_BPP=16' -I"C:/Users/Administrator/workspace/Test_SW4STM33/FATFS/Target" -I"C:/Users/Administrator/workspace/Test_SW4STM33/FATFS/App" -I"C:/Users/Administrator/workspace/Test_SW4STM33/Core/Inc" -I"C:/Users/Administrator/workspace/Test_SW4STM33/TouchGFX/target" -I"C:/Users/Administrator/workspace/Test_SW4STM33/USB_HOST/App" -I"C:/Users/Administrator/workspace/Test_SW4STM33/USB_HOST/Target" -I"C:/Users/Administrator/workspace/Test_SW4STM33/TouchGFX/generated/fonts/include" -I"C:/Users/Administrator/workspace/Test_SW4STM33/TouchGFX/generated/texts/include" -I"C:/Users/Administrator/workspace/Test_SW4STM33/TouchGFX/generated/images/include" -I"C:/Users/Administrator/workspace/Test_SW4STM33/TouchGFX/generated/gui_generated/include" -I"C:/Users/Administrator/workspace/Test_SW4STM33/TouchGFX/gui/include" -I"C:/Users/Administrator/workspace/Test_SW4STM33/Middlewares/ST/TouchGFX/touchgfx/framework/include" -I"C:/Users/Administrator/workspace/Test_SW4STM33/Drivers/STM32F7xx_HAL_Driver/Inc" -I"C:/Users/Administrator/workspace/Test_SW4STM33/Drivers/STM32F7xx_HAL_Driver/Inc/Legacy" -I"C:/Users/Administrator/workspace/Test_SW4STM33/Middlewares/Third_Party/FatFs/src" -I"C:/Users/Administrator/workspace/Test_SW4STM33/Middlewares/Third_Party/FreeRTOS/Source/include" -I"C:/Users/Administrator/workspace/Test_SW4STM33/Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS" -I"C:/Users/Administrator/workspace/Test_SW4STM33/Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1" -I"C:/Users/Administrator/workspace/Test_SW4STM33/Middlewares/ST/STM32_USB_Host_Library/Core/Inc" -I"C:/Users/Administrator/workspace/Test_SW4STM33/Middlewares/ST/STM32_USB_Host_Library/Class/CDC/Inc" -I"C:/Users/Administrator/workspace/Test_SW4STM33/Drivers/CMSIS/Device/ST/STM32F7xx/Include" -I"C:/Users/Administrator/workspace/Test_SW4STM33/Drivers/CMSIS/Include" -I"C:/Users/Administrator/workspace/Test_SW4STM33/Middlewares/ST/TouchGFX/touchgfx/framework/include/platform/hal/simulator/sdl2/vendor" -Og -g3 -Wall -fmessage-length=0 -ffunction-sections -c -fno-exceptions -fno-rtti -MMD -MP -MF"Middlewares/ST/TouchGFX/touchgfx/framework/source/platform/driver/touch/SDL2TouchController.d" -MT"Middlewares/ST/TouchGFX/touchgfx/framework/source/platform/driver/touch/SDL2TouchController.o" -o "Middlewares/ST/TouchGFX/touchgfx/framework/source/platform/driver/touch/SDL2TouchController.o" "../Middlewares/ST/TouchGFX/touchgfx/framework/source/platform/driver/touch/SDL2TouchController.cpp"
In file included from C:/Users/Administrator/workspace/Test_SW4STM33/Middlewares/ST/TouchGFX/touchgfx/framework/include/platform/hal/simulator/sdl2/vendor/SDL2/SDL_video.h:31:0,
from C:/Users/Administrator/workspace/Test_SW4STM33/Middlewares/ST/TouchGFX/touchgfx/framework/include/platform/hal/simulator/sdl2/HALSDL2.hpp:22,
from ../Middlewares/ST/TouchGFX/touchgfx/framework/source/platform/driver/touch/SDL2TouchController.cpp:17:
C:/Users/Administrator/workspace/Test_SW4STM33/Middlewares/ST/TouchGFX/touchgfx/framework/include/platform/hal/simulator/sdl2/vendor/SDL2/SDL_stdinc.h:261:50: error: size of array 'SDL_dummy_enum' is negative
typedef int SDL_dummy_ ## name[(x) * 2 - 1]
^
C:/Users/Administrator/workspace/Test_SW4STM33/Middlewares/ST/TouchGFX/touchgfx/framework/include/platform/hal/simulator/sdl2/vendor/SDL2/SDL_stdinc.h:290:1: note: in expansion of macro 'SDL_COMPILE_TIME_ASSERT'
SDL_COMPILE_TIME_ASSERT(enum, sizeof(SDL_DUMMY_ENUM) == sizeof(int));
^~~~~~~~~~~~~~~~~~~~~~~
Middlewares/ST/TouchGFX/touchgfx/framework/source/platform/driver/touch/subdir.mk:21: recipe for target 'Middlewares/ST/TouchGFX/touchgfx/framework/source/platform/driver/touch/SDL2TouchController.o' failed
make: *** [Middlewares/ST/TouchGFX/touchgfx/framework/source/platform/driver/touch/SDL2TouchController.o] Error 1
I have no idea how to fix this error.
Was your compiler able to find a path to the SDL2 folder? Do you have any ideas why you are able to build your project and I cannot build mine?
Thank you in advance for any further help you can provide!
2018-12-10 10:41 PM
exclude file platform/driver/touch/SDL2TouchController.cpp from compilation