2022-07-20 2:54 AM
Hello,
I'm currently in the process of creating a Custom Container top bar (Banner) with a clock (and other values like text with wildcard) that propagates through the screens. But I hit a dead end days ago and I cannot find the solution.
Step 1: The fake hardware sets the time
Step 2: I propagate it to the model
Step 3: I propagate it to the presenter of the first screen
Step 4 : I propagate it to the custom container Banner present on all my screens. → That's where I have my problem.
The problem:
The clock updates to the time I set in my Hardware for a second, then the next second (60 ticks), it is set to 00:00:01 (first second passed) and when I change screen, the clock propagates as I want to but with the basis of the first screen aka 00:00:01.
I've based the application mainly on this ST post and glanced info in other posts but I can't manage to make my app work :
Here's the Screen1View.cpp code where I update my Clock in the Banner.
Screen1View::Screen1View()
{
}
void Screen1View::setupScreen()
{
Screen1ViewBase::setupScreen();
clockscreen1 = presenter->getTimePres();
banner.setTime(clockscreen1);
}
void Screen1View::tearDownScreen()
{
Screen1ViewBase::tearDownScreen();
}
Here's my Custom container BannerBase.cpp
BannerBase::BannerBase()
{
setWidth(289);
setHeight(72);
digitalClock.setPosition(0, 0, 289, 72);
digitalClock.setColor(touchgfx::Color::getColorFromRGB(0, 0, 0));
digitalClock.setTypedText(touchgfx::TypedText(T___SINGLEUSE_BIUJ));
digitalClock.displayLeadingZeroForHourIndicator(true);
digitalClock.setDisplayMode(touchgfx::DigitalClock::DISPLAY_24_HOUR);
digitalClock.setTime24Hour(10, 10, 0);
add(digitalClock);
}
BannerBase::~BannerBase()
{
}
void BannerBase::initialize()
{
}
Here's the Banner.hpp
class Banner : public BannerBase
{
public:
Banner();
virtual ~Banner() {}
virtual void initialize();
virtual void handleTickEvent();
virtual void setTime(MyClock value);
protected:
int tickCounter;
int digitalHours;
int digitalMinutes;
int digitalSeconds;
};
And the Banner.cpp
Banner::Banner()
{
touchgfx::Application::getInstance()->registerTimerWidget(this);
// digitalHours = digitalClock.getCurrentHour();
// digitalMinutes = digitalClock.getCurrentMinute();
// digitalSeconds = digitalClock.getCurrentSecond();
digitalClock.setTime24Hour(digitalHours, digitalMinutes, digitalSeconds);
}
void Banner::initialize()
{
BannerBase::initialize();
}
// Rajout Clock
void Banner::handleTickEvent()
{
tickCounter++;
if (tickCounter % 60 == 0)
{
if (++digitalSeconds >= 60)
{
digitalSeconds = 0;
if (++digitalMinutes >= 60)
{
digitalMinutes = 0;
if (++digitalHours >= 24)
{
digitalHours = 0;
} // End hours
} // End minutes
} // End seconds
// Update the clocks
digitalClock.setTime24Hour(digitalHours, digitalMinutes, digitalSeconds);
} // End modulo
}
void Banner::setTime(MyClock value)
{
digitalClock.setTime24Hour(value.hour, value.minute, value.second);
}
My guess is I would need to put something in the initialize of the Banner but I cannot find what exactly or why my clock is set back to 00:00:00 ... probably related to
touchgfx::Application::getInstance()->registerTimerWidget(this);
digitalClock.setTime24Hour(digitalHours, digitalMinutes, digitalSeconds);
I also have a fear that the BannerBase will set my clock to 10:10:00 and I do not want that either. How can I prevent this?
If possible, I would like to keep using the registerTimerWidget since I don't wanna update each screen (there's a lot of them) I would only set up the time in my first screen. If really not possible, how can I set my 1st screen right (the time I asked in my hardware is set and not 00:00:00) and I'll save it to the model and update it in screen 2. And I fear the time I propagate it to the model and update it in screen 2, I would have missed some ticks so my time would begin to drift.
I have also read that it was planned to insert a feature in a new version of TouchGFX where we would be able to group functionalities used in several screens (like containers) to not repeat the code. Any news on this feature? It seems really interesting.
Thanks in advance for your answer,
Eve
Solved! Go to Solution.
2022-07-27 3:22 AM
Hello,
After trying different things, I finally succeeded on fixing your issues.
Your project is globally fine, I just had to correct small details. I will explain you what was wrong and what I had to add :
if (tickCounter % 60 == 0)
{
// -> Here
digitalSeconds = digitalClock.getCurrentSecond();
digitalMinutes = digitalClock.getCurrentMinute();
digitalHours = digitalClock.getCurrentHour();
//
if (++digitalSeconds >= 60)
{
digitalSeconds = 0;
if (++digitalMinutes >= 60)
{
digitalMinutes = 0;
if (++digitalHours >= 24)
{
digitalHours = 0;
} // End hours
} // End minutes
} // End seconds
// Update the clocks
digitalClock.setTime24Hour(digitalHours, digitalMinutes, digitalSeconds);
} // End modulo
void Screen1View::setupScreen()
{
Screen1ViewBase::setupScreen();
if(!presenter->isInitialized())
{
clockscreen1 = presenter->getTimePres();
banner.setTime(clockscreen1);
presenter->setInitialized();
}
}
I will join the fixed project to this post. Please check it and let me know if you have questions.
/Yoann
2022-07-25 1:43 AM
Hello @ELero.1 ,
Is it possible for you to share your project ?
That could help us a lot for trying to find how to fix your issue.
Thanks,
/Yoann
2022-07-25 3:49 AM
2022-07-26 3:00 AM
Hello,
I ran your project on my computer, and for me everything seems to work fine.
The clock is correctly propagated between all screens.
Could you please provide pictures of the display or a video of the issue you are noticing ?
Thank you,
/Yoann
2022-07-26 6:30 AM
Hello @Yoann KLEIN ,
Sure, here's some screencaps of the simulator.
Yes the propagation works fine, it's the clock I set that has a problem. I set with my fakehardware the clock to 08:25:36 in screen1.
It stays at that time for 1 second then it reverts back to 00:00:01
From there it continues counting like it should
When I change the screens it propagates well.
But that's not the time I wanted to set at the beginning. I wanted to start at 08:25:36 and start counting from there → 08:25:37 instead of 00:00:01
Kind regards,
Eve
2022-07-27 3:22 AM
Hello,
After trying different things, I finally succeeded on fixing your issues.
Your project is globally fine, I just had to correct small details. I will explain you what was wrong and what I had to add :
if (tickCounter % 60 == 0)
{
// -> Here
digitalSeconds = digitalClock.getCurrentSecond();
digitalMinutes = digitalClock.getCurrentMinute();
digitalHours = digitalClock.getCurrentHour();
//
if (++digitalSeconds >= 60)
{
digitalSeconds = 0;
if (++digitalMinutes >= 60)
{
digitalMinutes = 0;
if (++digitalHours >= 24)
{
digitalHours = 0;
} // End hours
} // End minutes
} // End seconds
// Update the clocks
digitalClock.setTime24Hour(digitalHours, digitalMinutes, digitalSeconds);
} // End modulo
void Screen1View::setupScreen()
{
Screen1ViewBase::setupScreen();
if(!presenter->isInitialized())
{
clockscreen1 = presenter->getTimePres();
banner.setTime(clockscreen1);
presenter->setInitialized();
}
}
I will join the fixed project to this post. Please check it and let me know if you have questions.
/Yoann
2022-07-27 3:28 AM
2022-07-27 5:07 AM
Hello @Yoann KLEIN ,
It works perfectly. Thank you so much!
Just a small question in Model.hpp you added this:
#include <touchgfx/containers/clock/DigitalClock.hpp>
touchgfx::DigitalClock digitalClock;
Why did you add those two lines? I didn't add it because I didn't understand what it was doing. It works perfectly fine without it though.
Kind regards,
Eve
2022-07-27 5:13 AM
Hello,
Sorry, I might have added that while testing stuff and forgot to delete it before sharing the new version of the project.
You can delete it of course.
/Yoann
2025-02-03 1:10 AM
Hello,
How can I use the image that is common to all screens, how can I call the widgets of one screen to another screen, so that only one time, I have to put that widget on one screen and I can access that widget on multiple screens. To reduce the memory consumption.
Thanks