2019-02-14 07:01 AM
I am attempting to setup the TouchGFX on a 32F746DISCOVERY Board with CubeMX and SW4STM32.
When I create the Board project in CubeMX, the stm32f7xx_hal_conf is empty.
I would have expected that the Peripherals would have some initialization code setup by Cube, but I am new to Cube so perhaps someone can point out if stm32f7xx_hal_conf needs to be setup by me or if its a bug in Cube.
Thanks
Martin
Solved! Go to Solution.
2019-02-14 11:16 AM
Hello,
OK, I have resolved this issue on Win 7.
I uninstalled Cube,
Re-installed JRE,
Installed CubeMx.
Now, I get a populated stm32f7xx_hal_conf.h file.
Thanks
2019-02-14 08:06 AM
Hello,
Please share your ioc file for check.
Kind Regards,
Imen
2019-02-14 08:30 AM
2019-02-14 11:16 AM
Hello,
OK, I have resolved this issue on Win 7.
I uninstalled Cube,
Re-installed JRE,
Installed CubeMx.
Now, I get a populated stm32f7xx_hal_conf.h file.
Thanks