Cube MX not generates lockDMAToFrontPorch(true);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-17 12:28 AM
Hello!
I have old project. It has file TouchGFXGeneratedHAL.cpp, where I can see code
void TouchGFXGeneratedHAL::initialize()
{
HAL::initialize();
registerEventListener(*(Application::getInstance()));
enableLCDControllerInterrupt();
enableInterrupts();
setFrameBufferStartAddresses((void*)0xD0000000, (void*)0xD0200000, (void*)0);
/*
* Set whether the DMA transfers are locked to the TFT update cycle. If
* locked, DMA transfer will not begin until the TFT controller has finished
* updating the display. If not locked, DMA transfers will begin as soon as
* possible. Default is true (DMA is locked with TFT).
*
* Setting to false to increase performance when using double buffering
*/
lockDMAToFrontPorch(true);
}
I updated CubeMX and TouchGFXdesigner to last version, and I saw
void TouchGFXGeneratedHAL::initialize()
{
HAL::initialize();
registerEventListener(*(Application::getInstance()));
enableLCDControllerInterrupt();
enableInterrupts();
setFrameBufferStartAddresses((void*)0xD0000000, (void*)0xD0200000, (void*)0);
}
String "lockDMAToFrontPorch(true);" lost.
And I see artifacts while widgeds moving.
A added string lockDMAToFrontPorch(true), artifacts disappeared.
But I need to put this string every time, I edit CubeMX project...
New version of TouchGFX not supports this option?
I found string "lockDMAToFrontPorch(false)" in file HALSDL2.cpp, but setting it to true has no effect.
Why?
- Labels:
-
STM32CubeMX
-
TouchGFX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-17 9:04 AM
Hi i see this too, but i mean this settings is for single buffering and in good double buffering is irelevant, then new remove it.
When you generate code with single buffer , yuo have this line back in code.
And i see artifacts too in new 4.15, then i stay use 4.13.
You can add this line to HAL file not generated
void TouchGFXHAL::initialize()
{
// Calling parent implementation of initialize().
//
// To overwrite the generated implementation, omit call to parent function
// and implemented needed functionality here.
// Please note, HAL::initialize() must be called to initialize the framework.
TouchGFXGeneratedHAL::initialize();
//add here
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-18 12:49 AM
Hi EEuge and MM.1,
Could you explain what artifacts you have seen with 4.15 ? Could you share some code or pictures ?
To try to replicate this issue could you tell us your two setups (which board, version of TouchGFX, STM32CubeProgrammer...) ?
/Romain
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-11 12:52 AM
Hi Romain !
I have encountered the same issue with our STM32F750 using : CubeMX : 6.91., CubeIDE :1.13.1 & touchGFX : 4.22
The LockDMA call is not inserted, but artifacts are present ie. if using a slider to change to alpha value on a box or even moving a small image. Looking around the forum it should not be nessesary to call the lockDMAToFrontPorch(true); routine. And it should also be costly performance wise.
Could there other setting that is needed to get rid of the call ?
800x480 RGB565 :
void TouchGFXGeneratedHAL::initialize()
{
HAL::initialize();
registerEventListener(*(Application::getInstance()));
setFrameBufferStartAddresses((void*)0xC0000000, (void*)0xC00BB800, (void*)0);
}
/Jakob