2024-11-01 12:55 PM - last edited on 2024-11-04 12:01 AM by mƎALLEm
Hi,
I am implementing a screen with particular number of flex buttons. The buttons are generated by my code and number of buttons change depending on some other variables. So far, I can create those flex buttons by code and see and touch them on the display. They change color when I touch them, so that I realise that buttons are functional. But of course, nothing happens when I touch them, because there are no callback functions. And I couldn't find a way how to implement callback function/functions for them.
Here is a part of my code, showing how I create those buttons:
for (uint8_t i=1; i<=numberoflines; i++)
{
Buttons[i].setBoxWithBorderPosition(0, 0, 337, 30);
Buttons[i].setBorderSize(0);
Buttons[i].setBoxWithBorderColors(touchgfx::Color::getColorFromRGB(0, 0, 0), touchgfx::Color::getColorFromRGB(150, 150, 150), touchgfx::Color::getColorFromRGB(80, 80, 80), touchgfx::Color::getColorFromRGB(150, 150, 150));
Buttons[i].setPosition(2, (i*30+5), 337, 30);
Buttons[i].invalidate();
scrollableContainer1.add(Buttons[i]);
Line[i].setPosition(42, (i*30+10), 294, 19);
Line[i].setColor(touchgfx::Color::getColorFromRGB(255, 255, 255));
Line[i].setLinespacing(0);
Unicode::snprintf(TextBuffer[i], 100, "TEST TEST %d %d", i, i);
Line[i].setWildcard(TextBuffer[i]);
Line[i].setTypedText(touchgfx::TypedText(1));
Line[i].invalidate();
scrollableContainer1.add(Line[i]);
}
scrollableContainer1.invalidateContent();
scrollableContainer1.invalidate();
Could you please help me to implement callback functions for those buttons?
Many thanks.
Solved! Go to Solution.
2024-11-04 02:42 AM
Hello @NGune.1 ,
The function that you'd probably need to use is the setAction().
If you create a flexButton within TouchGFX Designer and generate code, you'll notice this in the Screen1ViewBase.cpp :
Screen1ViewBase::Screen1ViewBase() :
flexButtonCallback(this, &Screen1ViewBase::flexButtonCallbackHandler)
{
...
flexButton1.setAction(flexButtonCallback);
...
}
And the callback :
void Screen1ViewBase::flexButtonCallbackHandler(const touchgfx::AbstractButtonContainer& src)
{
if (&src== &flexButton1)
{
//Interaction1
//When flexButton1 clicked call virtual function
//Call function1
function1();
}
}
function1 being implemented in the user code.
I invite you to look at our YouTube video in which we detail the generated code of a button.
2024-11-04 12:03 AM
2024-11-04 02:42 AM
Hello @NGune.1 ,
The function that you'd probably need to use is the setAction().
If you create a flexButton within TouchGFX Designer and generate code, you'll notice this in the Screen1ViewBase.cpp :
Screen1ViewBase::Screen1ViewBase() :
flexButtonCallback(this, &Screen1ViewBase::flexButtonCallbackHandler)
{
...
flexButton1.setAction(flexButtonCallback);
...
}
And the callback :
void Screen1ViewBase::flexButtonCallbackHandler(const touchgfx::AbstractButtonContainer& src)
{
if (&src== &flexButton1)
{
//Interaction1
//When flexButton1 clicked call virtual function
//Call function1
function1();
}
}
function1 being implemented in the user code.
I invite you to look at our YouTube video in which we detail the generated code of a button.
2024-11-04 03:05 AM
Hi Mr. Soykurt,
First of all, thank you for your reply.
Using the Designer, I previously generated flex buttons and assigned them functions via interactions, as you mentioned above. They work properly.
But, I am not generating those buttons, mentioned in the question, via TouchGFX Designer, that is where my problem begins. There will be unknown number of buttons in the project. That's why I am generating those buttons in my code. Let say, in Screen1View, in a for loop. The buttons are generated in the loop without problem. And even, when I touch them on the display, I see that they respond and change color.
However, I can't assign them functions. That is exactly my question. I couldn't find a way to assign them functions in the code.
Could you please re-think about the question?
Many thanks and kind regards.
Namik
2024-11-04 05:51 AM
Hi again,
By inspecting the answer, provided by Mr. Soykurt, more carefully, I managed to solve the issue.
What I did is (to be reference for other people):
I placed this piece of code in the beginning.
ProgView::ProgView() :
flexButtonCallback(this, &ProgView::flexButtonCallbackHandler)
{
for (uint8_t i=1; i<=numberoflines; i++)
{
Buttons[i].setAction(flexButtonCallback);
}
}
And then wrote the following functions:
void ProgView::flexButtonCallbackHandler(const touchgfx::AbstractButtonContainer& src)
{
for (uint8_t i = 1; i <= numberoflines; i++)
{
if (&src== &Buttons[i])
{
SelectedLine(i);
}
}
}
void ProgView::SelectedLine(uint8_t line)
{
Unicode::snprintf(DescTextBuffer, DESCTEXT_SIZE, "Line %d Selected", line);
DescText.invalidate();
}
Of course, the function prototypes are written in the ProgView.hpp :
class ProgView : public ProgViewBase
{
public:
virtual void SelectedLine(uint8_t line);
protected:
touchgfx::Callback<ProgView, const touchgfx::AbstractButtonContainer&> flexButtonCallback;
void flexButtonCallbackHandler(const touchgfx::AbstractButtonContainer& src);
}
So, the problem is solved.
Thank you very much.
2024-11-04 08:43 AM
Hello @NGune.1,
Indeed, the example I provided was only for showing what was missing in your code. What is generated by TouchGFX Designer needs to be written in your user code if you create your button through code of course. But I'm happy to hear that you managed to solve your problem :)