2024-10-14 2:48 AM
Is it possible to create a custom widget in touchgfx using code, specifically in stm32cubeide? I would like to start with a blank screen and add a custom widget that I design through code. What are the steps involved in achieving this, including creating the widget class, integrating it into the screen, and ensuring it functions correctly?
Solved! Go to Solution.
2024-10-14 6:00 AM
Hello @Ismails and welcome to the community!
To create a custom widget, the simplest way is to open TouchGFX Designer, create a new project.
Then, on your application, just go to the "Containers" tab and click on the "+" icon :
Then, you can add shapes, images, etc that you will need for your custom widget.
Then, click on "Generate code":
Then you can open the folder where your project is inside your favorite text editor or IDE (in that case, STM32CubeIDE):
The custom container code will be under TouchGFX => gui => source => container.
From there you can code custom behavior.
I hope this help!
If this comment answers your question, I invite you to select it as "best answer". :smiling_face_with_smiling_eyes:
Regards,
2024-10-14 6:00 AM
Hello @Ismails and welcome to the community!
To create a custom widget, the simplest way is to open TouchGFX Designer, create a new project.
Then, on your application, just go to the "Containers" tab and click on the "+" icon :
Then, you can add shapes, images, etc that you will need for your custom widget.
Then, click on "Generate code":
Then you can open the folder where your project is inside your favorite text editor or IDE (in that case, STM32CubeIDE):
The custom container code will be under TouchGFX => gui => source => container.
From there you can code custom behavior.
I hope this help!
If this comment answers your question, I invite you to select it as "best answer". :smiling_face_with_smiling_eyes:
Regards,