Skip to main content
FLine.1
Associate II
December 25, 2020
Solved

Control Pins and communicate via usart issue

  • December 25, 2020
  • 22 replies
  • 4351 views

Helleo,

I am newbie in Touchgfx and I try developing first project.

I am willing to data transfer stm32746 to pc via usart and control pins.

When I click the button stm doesnt send data via usart or stm doesnt control pins.

Screen1View.cpp codes:

#include <gui/screen1_screen/Screen1View.hpp>
#include "stm32f7xx_hal.h"
extern UART_HandleTypeDef huart2;
 
Screen1View::Screen1View()
{
 
}
 
void Screen1View::setupScreen()
{
 Screen1ViewBase::setupScreen();
}
 
void Screen1View::tearDownScreen()
{
 Screen1ViewBase::tearDownScreen();
}
 
void Screen1View::led_on()
{
 
/*	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1, GPIO_PIN_SET);
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1|GPIO_PIN_4|GPIO_PIN_2|GPIO_PIN_5
	 |GPIO_PIN_3, GPIO_PIN_SET);
*/
	//HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_5);
	//HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_6);
 // textArea1.setVisible(true);
	char com_cevap[12] ="adc_veri\r\n ";
	HAL_UART_Transmit(&huart2, (uint8_t *) &com_cevap, 12, 200);
 btndurum.setAlpha(254);
 btndurum.invalidate();
 
}
 
void Screen1View::led_off()
{
/*	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1|GPIO_PIN_4|GPIO_PIN_2|GPIO_PIN_5
	 |GPIO_PIN_3, GPIO_PIN_RESET);
*/
	//HAL_GPIO_WritePin(GPIOD, GPIO_PIN_5, GPIO_PIN_RESET);
	//HAL_GPIO_WritePin(GPIOD, GPIO_PIN_6, GPIO_PIN_RESET);
 btndurum.setAlpha(50);
 btndurum.invalidate();
 
}

0693W000006GtqXQAS.png 

please tell me whats wrong? Could i control pins or data transfer in button click?

I use STMCubeIDe 1.5.1, Visual Studio 2019 and last framework.TouchGfx 4.15

This topic has been closed for replies.
Best answer by MM..1

DISCO-F746NG | Mbed read image with pinout description

22 replies

MM..1
Super User
December 27, 2020

You need debug your code, because from your info we cant help.

Yes you can control activated GPIO , or use quick transfers. For slow is better use IT DMA or next thread in RTOS.

FLine.1
FLine.1Author
Associate II
December 30, 2020

hello,

If you have sample project about uart, please share it.

I added my debug file. How can i get sample videos touchgfx.

MM..1
Super User
December 30, 2020

You missunderstand me , Debug folder, that you zip is totaly unusable for help you.

FLine.1
FLine.1Author
Associate II
December 30, 2020

i added . if you have a video for education and share i appreciate.

MM..1
Super User
December 30, 2020

Try this in your main.c

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
char giden[10]="";
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
....
....
 
void StartTaskUart(void const * argument)
{
 /* USER CODE BEGIN StartTaskUart */
 /* Infinite loop */
 for(;;)
 {
	 if(giden[0]!=0) {
		 HAL_UART_Transmit(&huart2, (uint8_t *)giden,10,30);
		 giden[0]=0;
	 }
 
 osDelay(10);
 }
 /* USER CODE END StartTaskUart */
}
 

and screenview.cpp

#include <gui/screen1_screen/Screen1View.hpp>
#include "stm32f7xx_hal.h"
#include "string.h"
 
extern char giden[];
 
Screen1View::Screen1View()
{
 
}
 
void Screen1View::setupScreen()
{
 Screen1ViewBase::setupScreen();
}
 
void Screen1View::tearDownScreen()
{
 Screen1ViewBase::tearDownScreen();
}
 
void Screen1View::veri_gonder()
{
	//HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_5);
	//HAL_Delay(200); ??? DONT USE DELAYS IN GUI !!!
	strcpy(giden, "start\n\r");	// checked in thread and send
 
}
 
void Screen1View::veri_stop()
{
	//HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_6);
	//	HAL_Delay(200);
//	char giden[10]="stop\n\r";
	if(giden[0]==0) strcpy(giden, "stop\n\r");
}
 

zzzzz
Senior
December 30, 2020

When include some C headers in Cpp, put them inside external C. like this:

#include <gui/screen1_screen/Screen1View.hpp>

extern "C"

{

#include "stm32f7xx_hal.h"

#include "cmsis_os.h"

#include "UART.h" // put huart2 here

}

...

Then debug it, make sure HAL_UART_Transmit in your button callback is being called.

MM..1
Super User
December 30, 2020

Yes and when you try call it directly include extern, not create new.

UART_HandleTypeDef huart2; is new empty handle

instead use

extern UART_HandleTypeDef huart2;

or with extern "C" as writed zzzzz

FLine.1
FLine.1Author
Associate II
January 3, 2021

Hello

Thank you for replies.

I created new project and added two button with two interaction.

I set uart2 D5 and D6 pins.115200 baud and polling connecting not IT or DMA.

I coded like you but same result . i cant send data from stm32746 to pc via uart.

main.c

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
char giden[10] = "adbcde\r\n";
 
/* USER CODE END 0 */
 
static void MX_USART2_UART_Init(void)
{
 
 /* USER CODE BEGIN USART2_Init 0 */
 
 /* USER CODE END USART2_Init 0 */
 
 /* USER CODE BEGIN USART2_Init 1 */
 
 /* USER CODE END USART2_Init 1 */
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART2_Init 2 */
 
 /* USER CODE END USART2_Init 2 */
 
}

uart task i created in main.c

/* USER CODE END Header_StartTask_Uart */
void StartTask_Uart(void const * argument)
{
 /* USER CODE BEGIN StartTask_Uart */
 /* Infinite loop */
 for(;;)
 {
	 if (giden[0] != 0) {//icinde deger varsa
		 HAL_UART_Transmit(&huart2, (uint8_t *)giden, 10 ,30);
		 giden[0] = 0;
 
	}
 
 osDelay(1000);
 }
 /* USER CODE END StartTask_Uart */
}

screen1view.cpp

#include <gui/screen1_screen/Screen1View.hpp>
/*
extern "C"
{
	#include "stm32f7xx_hal.h"
	#include "cmsis_os.h"
	UART_HandleTypeDef huart2;
}
*/
 
#include "string.h"
 
extern char giden[];
 
Screen1View::Screen1View()
{
 
}
 
void Screen1View::setupScreen()
{
 Screen1ViewBase::setupScreen();
}
 
void Screen1View::tearDownScreen()
{
 Screen1ViewBase::tearDownScreen();
}
 
void Screen1View::basla()
{
	strcpy(giden, "basla\n\r");
	btnBasla.invalidate();
 
}
 
void Screen1View::bitir()
{
	if (giden[0] == 0) {
		strcpy(giden, "durdu\n\r");
 
	}
	btn_bitir.invalidate();
}

0693W000006HKpqQAG.png0693W000006HKplQAG.png0693W000006HKpgQAG.png

zzzzz
Senior
January 3, 2021
  1. I don't see any reason you need that UART task. You can do everything in your button callbacks. If you have to do it that way, please suspend the UART task when doing string copy or use a semaphore.
  2. You are not coded as I suggested, string.h is C header, need to move it to extern C. I see the whole extern c is commented out, have a problem to use it?
  3. How's your debug? As I said before, Is UART transmit function get called? if so, what data in the buffer?
zzzzz
Senior
January 3, 2021

I just reviewed your code, my code would like this:

  1. #include <gui/screen1_screen/Screen1View.hpp>
  2.  
  3. extern "C"
  4. {
  5. #include "stm32f7xx_hal.h"
  6. #include "main.h" // add extern UART_HandleTypeDef huart2 and extern char giden[10] to main.h
  7. #include "string"
  8. }
  9.  
  10. void Screen1View::basla()
  11. {
  12. strcpy(giden, "basla\n\r");
  13. HAL_UART_Transmit(&huart2, (uint8_t *)giden, 10 ,30);
  14. //btnBasla.invalidate(); // don't need this funciton
  15.  
  16. }

This shows how to use a buffer created in C file in Cpp file. Anything you created in C file, you need put them in extern C when you try using them in Cpp.

In your case, code in button callback could be as simple as this:

  1. void Screen1View::basla()
  2. {
  3. HAL_UART_Transmit(&huart2, (uint8_t *)"basla\n\r", 10 ,30);
  4. }

MM..1
Super User
January 3, 2021

@zzzzz​ Yes this work too, but only for short strings for example on 115200 to 100 chars. Then with bigger data you need task.

@FLine.1​  

And i see you maybe have problem on PC COM port , not in your code.

Please check with scope connected to TX signal.

And for connect to PC you need converting 3,3V TTL to RS232 . You cant connect directly. Plus your PC COM software must be properly set.

FLine.1
FLine.1Author
Associate II
January 3, 2021

Mr zzzz

Thank you for reply. it is crazy me.

I debug project STM32CubeIDE 1.5.1 . I suspend this tiime but result is same.

What do you mean UART transmit function callback?

If you have time you can remote connection my pc with anydesk. Anydesk number:205 312 968

I liked that last one: main.c

/* USER CODE END Header_StartTask_Uart */
void StartTask_Uart(void const * argument)
{
 /* USER CODE BEGIN StartTask_Uart */
 /* Infinite loop */
 for(;;)
 {
	 if (giden[0] != 0) {//icinde deger varsa
		 HAL_UART_Transmit_IT(&huart2, (uint8_t *)giden, 10 );
		 giden[0] = 0;
 
	}
 
 osDelay(1000);
 }
 /* USER CODE END StartTask_Uart */
}
 
 

screenview.cpp:

#include <gui/screen1_screen/Screen1View.hpp>
 
extern "C"
{
	#include "main.h"
	#include "stm32f7xx_hal.h"
	#include "cmsis_os.h"
	UART_HandleTypeDef huart2;
	#include "string.h"
	osThreadId Task_UartHandle;
	//osThreadDef(Task_Uart, StartTask_Uart, osPriorityHigh, 0, 128);
 
}
 
 
 
 
extern char giden[];
 
Screen1View::Screen1View()
{
 
}
 
void Screen1View::setupScreen()
{
 Screen1ViewBase::setupScreen();
}
 
void Screen1View::tearDownScreen()
{
 Screen1ViewBase::tearDownScreen();
}
 
void Screen1View::basla()
 
{
	osThreadSuspend(Task_UartHandle); //Task_UartHandle
	strcpy(giden, "basla\n\r");
	btnBasla.invalidate();
	osThreadResume(Task_UartHandle);
 
}
 
void Screen1View::bitir()
{
	if (giden[0] == 0) {
		strcpy(giden, "durdu\n\r");
 
	}
	btn_bitir.invalidate();
}

 0693W000006HLQrQAO.jpg

FLine.1
FLine.1Author
Associate II
January 3, 2021

Hello

I changed code like that but result is same.

It is crazy me. I suspend and resume task this time.

If you have time you can remote desktop my pc via Any desk :205 312 968

#include <gui/screen1_screen/Screen1View.hpp>
 
extern "C"
{
	#include "main.h"
	#include "stm32f7xx_hal.h"
	#include "cmsis_os.h"
	UART_HandleTypeDef huart2;
	#include "string.h"
	osThreadId Task_UartHandle;
	//osThreadDef(Task_Uart, StartTask_Uart, osPriorityHigh, 0, 128);
 
}
 
 
 
 
extern char giden[];
 
Screen1View::Screen1View()
{
 
}
 
void Screen1View::setupScreen()
{
 Screen1ViewBase::setupScreen();
}
 
void Screen1View::tearDownScreen()
{
 Screen1ViewBase::tearDownScreen();
}
 
void Screen1View::basla()
 
{
	osThreadSuspend(Task_UartHandle); //Task_UartHandle
	strcpy(giden, "basla\n\r");
	btnBasla.invalidate();
	osThreadResume(Task_UartHandle);
 
}
 
void Screen1View::bitir()
{
	if (giden[0] == 0) {
		strcpy(giden, "durdu\n\r");
 
	}
	btn_bitir.invalidate();
}
/* USER CODE END Header_StartTask_Uart */
void StartTask_Uart(void const * argument)
{
 /* USER CODE BEGIN StartTask_Uart */
 /* Infinite loop */
 for(;;)
 {
	 if (giden[0] != 0) {//icinde deger varsa
		 HAL_UART_Transmit_IT(&huart2, (uint8_t *)giden, 10 );
		 giden[0] = 0;
 
	}
 
 osDelay(1000);
 }
 /* USER CODE END StartTask_Uart */
}

0693W000006HLRBQA4.jpg

FLine.1
FLine.1Author
Associate II
January 3, 2021

0693W000006HLRLQA4.png

MM..1
Super User
January 3, 2021

Seems you have converter, but scope ?