2023-04-03 11:17 AM
Hi!
I'm getting 2 round displays up and running using tGFX on an STM32F767 (custom board, external SDRAM and QSPI)
I think almost everything is running but I have some weird artifacts. the clearest I can show is the color wheel test.
While the image is 24-bit and the display is 18-bit I wonder why I see the clear lines across the display (Please disregard the red stripe horisontally - that's a smudge on the protective film)
To me it would seem like something like a rounding of the color information but that would make much more sense if I was coming from less than 18-bit.
Anyone who can offer some insights here or point me in a direction? I tried with a real image and certain colors just get REALLY wonky..
Solved! Go to Solution.
2025-02-16 10:40 AM
Hi,
I am also trying st7701s using rgb and spi 9-bit.
i facing an issues of getting vertical bands when i try to draw horizontal lines.
have you experienced any such issue or suggest some reason.
Regards
Ajay Sharma
2025-08-23 12:36 AM
thanks for sharing
2025-09-18 4:24 AM - edited 2025-09-18 4:26 AM
Hi,
I am using STM32H723ZG controller with 268*800 resolution display which has ST7701 driver IC and using 9bit SPI, I configured all the necessary parameter but i am getting few lines on the display, but i am not able it figure it out what actually I made wrong. If anyone had idea on this please reply on this issue for more information i have added the image of LCD where i am getting few lines.