2023-06-20 04:00 AM
Hello, I have trouble cannot open apps Touchgfx 4.18.1 Designer in Windows. Any Solution? Thanks you
Solved! Go to Solution.
2023-07-03 02:42 AM
Hello @DPutr.1,
It's not difficult to upgrade your version project. You just need to open it in a higher version of TouchGFX and regenerate code from it. If it's a TBS, you also need to open the .ioc file of your project and regenerate code on STM32CubeMX.
2023-06-20 04:51 AM
Hello @DPutr.1 ,
Could you send us the log file located at the path mentioned in the error message please?
Also, we would recommend you to use 4.22.0 version of TouchGFX that we released yesterday :) It's much more stable, and complete solution than the 4.18.1. Take a look at this post.
/Osman
2023-06-20 08:13 PM
2023-06-20 08:41 PM
previously it worked , yesterday I was in debug mode to see the program run . suddenly my laptop blue screen and restart again. when I use it again it looks like this (I attached the view to stm32cubeide) and the touchgfx and apps files can't be used. any suggestions?can it be fixed?
2023-07-03 02:42 AM
Hello @DPutr.1,
It's not difficult to upgrade your version project. You just need to open it in a higher version of TouchGFX and regenerate code from it. If it's a TBS, you also need to open the .ioc file of your project and regenerate code on STM32CubeMX.
2023-07-03 02:48 AM - edited 2023-07-03 02:48 AM
I don't know what happened here, but it seems that the upgrade didn't complete properly. You can maybe try to revert your project to its original version if you version controlled it and try to upgrade again. Else, you could open the touchgfx file with a text editor and manually type the touchgfx version in it (last 3 lines of the file).