cancel
Showing results for 
Search instead for 
Did you mean: 

Can we set the Number of Data Points in Dynamic Graph widget dynamically during run time?

BParh.1
Senior III

So in TouchGFX designer, when we choose Dynamic Graph widget, we can input the number of data points. Let's say originally we set as 100 data points, but later we want to increase this, can we do this?

Also, is it really possible to increase X axis range without increasing the data point?

1 REPLY 1
ktrofimo
Senior III

Look at sources of Graph and you will see that there is no such functionality. Data is stored in an array of fixed length.