2020-09-24 11:52 AM
Hi,
I try to build a TouchGFX project with the CubeIDE but during compilation I always get weird errror messages like that:
./TouchGFX/touchgfx/os/OSWrappers.cpp:1:10: fatal error: touchgfx/framework/include/touchgfx/hal/OSWrappers.hpp: No such file or directory
This file is definitely in the project (just like the others which create errors as well). The shortkey F3 guides me to the file. So CubeIDE in principle knows where to find it.
I already included the path - see attachment.
I'm using CubeIDE1.4.2 and TouchGFX 4.13. I know that they are not compatibel but I can't open TouchGFX 4.14. Neither manually nor automatically.
Thanks
Gerhard
2020-09-25 6:38 AM
Hello,
Could you check if the library is correctly indicated in the libraries and library path tab ?
/Alexandre
2020-09-26 10:51 AM
Hi Alexandre,
indicating libraries and library path manually doesn't help. Now I reinstalled CubeIDE and repeated it, but that didn't help as well. Creating a TouchGFX with CubeIDE still leads to weird errrors that files can't be found which are definitely defined..
Implementing a Project which was created by TouchGFX works but this shouldn't be the workflow...
Best Regards
Gerhard
2020-09-28 12:26 AM
Could you enclose your project so that I can have a look and try to see what is the problem ?
It's definitely possible to create a project from scratch using CubeMX and TouchGFX so there must be something not correctly done in your project.
What board are you working on ? If it is a board that we support, then the normal workflow is to use the Application Template. If not a board we support but very similar (same MCU family), using the Application Template of the one we support as help is the best approach.
And if it is completely different, doing it from scratch is the right way.
/Alexandre
2020-09-28 8:47 AM
2020-09-29 12:13 AM
Why don't you want to use the Application template for F746G-DISCO ? I guess you don't if you have such an error.
Also I didn't see that you couldn't open 4.14, have you tried reinstalling it ?
/Alexandre
2020-09-29 1:59 AM
Hi Alexandre,
I'm a little bit confused. First you told me that creating a TouchGFX project with CubeIDE should work and now you recommend to use the TouchGFX template for F746-DISCO in order not to get any errors?
I created this project with CubeIDE 1.4.0 the following way:
after these various steps I should have a working project in CubdIDE? right?
I reinstalled CubeIDE 1.4.0. Since TouchGFX 4.14 is part of it I guess that TouchGFX 4.14 is reinstalled as well.
Best Regards
Gerhard
2020-09-29 2:25 AM
When did I say you could create a TouchGFX project with CubeIDE ? I don't recall saying it and I will never because I will always recommend using the Application Template if there is one.
/Alexandre
2020-09-29 2:28 AM
There is one part that we are not on the page I believe, when I say using CubeMX I don't mean using it with CubeIDE.
CubeMX works as a standalone software and from my experience in graphics you should prefer using CubeMX this way and CubeIDE as a simple IDE as it supposed to be. This is how we develop Application Templates so I can guarantee a working project with this workflow.
/Alexandre
2020-10-04 6:47 AM
I am getting the same error messages that files are missing but I can view the files when I click on the #include-Line and press F3.
I'm using the CubeIDE Version 1.4.2 with TouchGFX-Version 4.14, as well as CubeMX Version 6.0.1
Steps to reproduce the error:
This produces the error-messages attached in file "CubeIDE_TouchGFXErrors"
If I use the method Alexandre suggested, I get the errors attached in File CubeMX_TouchGFXErrors.
Steps to reproduce these error-messages:
This is basically exactly the sequence of steps shown in several Videos, including official videos made by STM.
The only way I can currently get a working code is to use the TouchGFX Designer and create a project with it that I import into CubeIDE. This is nice to experiment with and to see what TouchGFX can do (which is impressive and one of the reasons why I'm using ST Chips), but pretty much useless if I want to program my own hardware or talk to pieces of external hardware connected to the Discovery Board.
Does anyone have ideas on how to fix these problems?
Btw. I think it would help a lot of people if there was a simple step by step tutorial on how to implement drivers for one of the cheap ILI9341 Display-Modules that only offer SPI-Connection and are used basically everywhere in the Arduino Community.