cancel
Showing results for 
Search instead for 
Did you mean: 

build error

ferdlf
Associate III

I got a problem when building the project in the CubeIDE.
problem 1.png

According to the console, the function "function1" is not declared, but in the .hpp it is.
problem 2.png
I think the .cpp is not realizing that the .hpp is changing.
Here, when I use the content assit, function1 doesnt show up.

ferdlf_0-1706990428429.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

You need to save the Screen1View.hpp file before the IDE will recognize the new function. The "*" in the filename indicates it has been modified without being saved.

TDK_0-1706991984722.png

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Guru

You need to save the Screen1View.hpp file before the IDE will recognize the new function. The "*" in the filename indicates it has been modified without being saved.

TDK_0-1706991984722.png

 

If you feel a post has answered your question, please click "Accept as Solution".