cancel
Showing results for 
Search instead for 
Did you mean: 

How to configure h745bit6 on CubeIde and TouchGFX

NguyenAnhHieu_
Visitor

Hello,

I am trying to configure the STM32H745BIT6 with the TouchGFX interface. However, during the process, I encountered an error when generating because the build could not find the libraries from TouchGFX.

I have attempted to add the include paths in "MCU/MPU Gcc Compiler" and "MCU/MPU G++ Compiler", but the issue persists. How should I specify the correct paths so that TouchGFX recognizes them? The build process is handled automatically by the app, and I am unsure how to intervene manually.

I have referred to the setup guide from this video: https://www.youtube.com/watch?v=SRQD8JMeg_k&t=2063s

I would appreciate any help.

Thank you!

 NguyenAnhHieu__0-1742528262114.png

2 REPLIES 2
NguyenAnhHieu_
Visitor

Hello everyone,

I am currently working on a project using the STM32H745BIT6 chip, which features dual cores (M7 and M4). I am aiming to set up an LCD interface using TouchGFX. However, I encountered a build error right after writing the initial lines of code— the compiler cannot find a required library.

I have already tried adding the necessary include paths in both the "MCU/MPU Gcc Compiler" and "MCU/MPU G++ Compiler" settings, but the error still persists. Additionally, I attempted various methods to add the ST libraries from the Middlewares package, yet nothing has resolved the issue.

Currently, I am using STM32CubeIDE 1.18 and TouchGFX 4.20.

I would greatly appreciate any help or suggestions to resolve this build error.

Thank you very much for your support!

NguyenAnhHieu__0-1742479151518.png

 

JJhin.1
Senior II

After generating project from CubeMX you need to generate GUI from TouchGFX designer. and after you have to compile the project in Cube ide