cancel
Showing results for 
Search instead for 
Did you mean: 

Bug in TouchGFX 4.24.2 Designer with Multiple Monitors on Windows 11

mArSat
Associate

I'm experiencing an issue with TouchGFX Designer 4.24.2 on Windows 11 when using multiple monitors. If I drag the window from the primary screen to the secondary one, parts of the interface disappear completely.

I have attached screenshots showing the issue before and after moving the window.

Could you please investigate this? Let me know if you need any additional details.

Thank you.

1 REPLY 1
GaetanGodart
ST Employee

Hello @mArSat ,

 

I am not able to reproduce the issue.

However, I can see that you are at position -31646; -32509 (1), also, I can see that your screen is moved to the top left corner (2).
You can try to used the buttons to center your design at the bottom of the screen (3).

 

If this comment answers your question, I invite you to select it as "best answer".

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)