2019-03-29 08:24 AM
2019-04-02 12:09 AM
Hi @Mon2,
Thanks. Thought i'd already fixed that. Will update asap.
2019-04-02 05:25 AM
Ah, i found the problem.
We changed the package manager to run on http:// and not https://. I've updated the article to reflect that, but here's the direct link.
2021-01-28 09:46 AM
URL is broken again
Edit: I can only see a simulator template on Touchgfx designer . I guess the broken URL is the reason.
2021-01-28 06:17 PM
same issue here also. perhaps the server is down. (didn't realize it was dependent on the internet for those...)
Bob
2021-01-28 11:38 PM
Hi @Ebby and @Bob Bailey yes this is the issue, the server seems to be down. We are working on it sorry.
Here is the link for now http://sw-center-st-com.s3-eu-west-1.amazonaws.com/touchgfx/pacman/packages.json.zip . Once you download the zip files/tpa you can add them to designer following this article.
EDIT: it seems to still not be working, but we are working on it...
/Romain
2021-01-29 12:23 AM
2021-01-29 01:11 AM
I thought we were not using zendesk anymore, what documents are you talking about ? I'll ask around
/Romain
2021-01-29 01:41 AM
There is something wrong with the redirect from packages.touchgfx.com to the package server (which is up). I'm working on resolving the issue with a team from ST.
If you let us know here which packages you need, Romain will provide the direct links :) And you can install those directly into the designer . Right @Romain DIELEMAN ?
/Martin
2021-01-29 01:44 AM
always Martin