2023-07-31 12:10 AM - edited 2023-07-31 12:49 AM
I am using external flash for TouchGFX resources and also for saveing some parameters. I am doing the saveing of parameters in runtime with following code (emulated eeprom is in external flash):
void eepromCtrl(){
uint8_t EEpromQueueFillLevel = uxQueueMessagesWaiting(Queue_To_EEpromHandle);
if((EEpromQueueFillLevel <= 0) || !enableEEpromWriting){
return;
}
baseType = xQueueReceive(Queue_To_EEpromHandle, &eepromQueueMsg, portMAX_DELAY);
semaphoreCount1 = osSemaphoreGetCount(binarySemaphorFlashHandle);
if ((baseType == pdPASS) && (eepromQueueMsg.id > 0)) {
// osSemaphoreAcquire(binarySemaphorFlashHandle, 0);
osKernelLock();
// Suspend necessary interrupts
HAL_DMA2D_Suspend(&hdma2d);
NVIC_DisableIRQ(DMA2D_IRQn);
NVIC_DisableIRQ(TIM5_IRQn);
// Perform flash write
stat = ExtFlash_Abort(&hqspi);
if(stat == EXT_FLASH_OK){
ee_status = EE_WriteVariable32bits(eepromQueueMsg.id,eepromQueueMsg.value);
}
if(ee_status != EE_OK){
writeFailedCount++;
}
// Perform flash cleanup if required
if (ee_status == EE_CLEANUP_REQUIRED) {
eepromCleanUpCount++;
ee_status = EE_CleanUp();
if (ee_status != EE_OK) {
eepromCleanUpFailCount++;
};
}
stat = ExtFlash_MemoryMap(&hqspi);
// check if enterd memory mapped went ok
if(stat != EXT_FLASH_OK){
enterMemmroyMapFailCount++;
while(stat != EXT_FLASH_OK){
stat = ExtFlash_MemoryMap(&hqspi);
enterMemmroyMapFailCount++;
osDelay(1);
}
}
// Resume interrupts
NVIC_EnableIRQ(TIM5_IRQn);
NVIC_EnableIRQ(DMA2D_IRQn);
HAL_DMA2D_Resume(&hdma2d);
osKernelUnlock();
eepromWriteCount++;
osSemaphoreRelease(binarySemaphorFlashHandle);
}
}
I want to have a binary semaphore that shoud be taken by touchgfx when it is accessing external flash and released when it is not. Where shoud I put this? I tried to do it in TaskEntry() but without success:
void TouchGFXHAL::taskEntry()
{
/* USER CODE BEGIN taskEntry step 1 */
/* USER CODE END taskEntry step 1 */
enableLCDControllerInterrupt();
enableInterrupts();
/* USER CODE BEGIN taskEntry step 2 */
/* USER CODE END taskEntry step 2 */
OSWrappers::waitForVSync();
backPorchExited();
/* USER CODE BEGIN taskEntry step 3 */
/* Enable the LCD, Send Display on DCS command to display */
/* USER CODE END taskEntry step 3 */
for (;;)
{
OSWrappers::waitForVSync();
semaphoreStatus = osSemaphoreAcquire(binarySemaphorFlashHandle, 0);
taskAliveCount[TASK_GUI_ID]++;
backPorchExited();
osSemaphoreRelease(binarySemaphorFlashHandle);
}
}
2023-07-31 4:47 AM
2023-07-31 5:48 AM - edited 2023-07-31 6:16 AM
I get error undefined reference to `eepromCtrl()'. My EndFrame() function looks like beloow. On top of TouchGFXHAL.cpp I also included my librarry.#include "emulated_eeprom.h" so the fuznction should be defined? I this some c++ thing?
void TouchGFXHAL::endFrame()
{
TouchGFXGeneratedHAL::endFrame();
enableEEpromWriting = true;
eepromCtrl();
//osSemaphoreRelease(binarySemaphorFlashHandle);
}