cancel
Showing results for 
Search instead for 
Did you mean: 

AVI video frame size supported by TouchGFX on STM32H747 ?

miker
Associate II

I use the platform of STM32H747 to play a video with AVI format, if the frame width*height=568*320, touchGFX can't play this and skip this function,  which type of resolution can be used for touchGFX on STM32H747 platform ?

 

1 REPLY 1
GaetanGodart
ST Employee

Hello @miker ,

 

When you talk about the frame, do you mean the display size or the video size?

Are you able to make other frame size work?

Can you share the video you want to play in .avi and perhaps in the original format (mp4 or other)?

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)