2022-07-31 4:32 AM
To customize a TouchGFX application created with the TouchGFXDesigner,
I am trying to create a screen with many circles that can be updated, for that I use an array to store the circles and the circles painters, but then when I try to access the methods of the widgets in the array doesn't seem to work.
A simple example could be:
in "screen1View.hpp" I declare an array to store the circles and the painters inside the view class:
touchgfx::Circle circleArray[] = {circle1, circle2, ...};
touchgfx::PainterRGB565 painterArray[] = {circle1Painter, circle2Painter};Then in "screen1View.cpp" I try to access the widgets in the array to change the color:
void Screen1View::action()
{
// ...
painterArray[0].setColor(touchgfx::Color::getColorFromRGB(255, 0, 0));
circleArray[0].invalidate();
}But this doesn't work, the color is not updated.
But instead if I directly use the widget instance like this:
void Screen1View::action()
{
// ...
circle1Painter.setColor(touchgfx::Color::getColorFromRGB(255, 0, 0));
circle1.invalidate();
}Then the color gets updated
I am not very experienced in C++ so could this be related to the language?
or can this be achieved in some other way?
Solved! Go to Solution.
2022-07-31 4:48 AM
Maybe this help you c++ - Passing an array of pointers to a Class Object - Stack Overflow
and cleaner is in hpp only declare without = {}... and assign in setupscreen.
2022-07-31 4:48 AM
Maybe this help you c++ - Passing an array of pointers to a Class Object - Stack Overflow
and cleaner is in hpp only declare without = {}... and assign in setupscreen.
2022-07-31 10:29 AM
Yeah, using an array of pointers to objects instead of an array of objects works.
Thanks