2017-02-03 5:40 AM
I have Nucleo-F767ZI board and want to use Arduino protoshield to ease making connections to a peripheral (I will solder 2x8 pin header to the shield and use a ribbon cable). However I cannot find any PDF on ST Zio connector, which will apparently be used by the Arduino shield. Where is the data?
Also, I'll be using DCMI and I'm worried that ST Zio will pin-collide with it. So it's about: which pins are used by ST Zio, particularly with Arduino shield?
Best regards,
Sebastian
#arduino #dcmi #pins #zioSolved! Go to Solution.
2017-02-03 6:03 AM
Hi Sebastian,
you can have the description of the ST Zio connector in the following document:
I hope this can help you.
Best Regards.
Marc.
2017-02-03 6:03 AM
Hi Sebastian,
you can have the description of the ST Zio connector in the following document:
I hope this can help you.
Best Regards.
Marc.
2017-02-03 6:07 AM
Hi Sebastian,
Did you checked the
(STM32 Nucleo-144 board)?Don't you find required details there?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-02-04 2:39 AM
Yes the details are there, thanks. Finding this through google is hard.
2017-02-04 8:30 AM
>>Finding this through google is hard.
In the sense of looking in the wrong pocket for your keys kind of way...
2020-12-21 8:51 PM
I have a NUCLEO-L552ZE-Q board, it was said it supports Arduino, ST Zio and morpho connectivity, and it was also said it has Arduino, Mbed and morpho connectivity. So, my question is "Is ST Zio corresponding to Mbed connectivity?"