cancel
Showing results for 
Search instead for 
Did you mean: 

About JPEG Codec decoding time length

NYana.1
Associate

Decoded VGA size JPEG images on STM32H750B-DK.

As a result of measuring the decoding processing time, it takes three times as long as the processing time of Application note.

I would like to know the reason why the processing time is so long.

Application Note : 4ms

Measured value  : 12ms

[Program]

HAL_JPEG_Decode_DMA(hjpeg ,(uint8_t *)JPEGSourceAddress ,CHUNK_SIZE_IN ,(uint8_t *)FrameBufferAddress ,CHUNK_SIZE_OUT);

[Reference]

AN4996 Application note

https://www.st.com/resource/en/application_note/dm00356635-hardware-jpeg-codec-peripheral-in-stm32f76-77xxx-and-stm32h743-53-45-55-47-57-50-a3-b3-b0xx-microcontrollers-stmicroelectronics.pdf

3.2 JPEG decoding performances 

 Product : STM32H743L

 Image resolution : VGA(640x480)

 Hardware decoding : 4ms

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0