cancel
Showing results for 
Search instead for 
Did you mean: 

Add name of container for items in screen

GMeta.1
Associate II

It would be useful if an item (widget) added to a screen which is a container, showed the name of the container in the properties window. I have a lot of different containers and if I need to make changes to the container, sometimes I have to go through almost the whole list of containers to find the one I need. If the properties window in the top right of the designer window showed the name of the container, then this would be easier

Maybe also a quicker way to jump to the container either from the screens tab (context menu for example) or via the widget properties window. It is useful btw having an appropriate icon for each widget in the screens tree because you can at least tell if it is a button, line, container etc

1 ACCEPTED SOLUTION

Accepted Solutions
LouisB
ST Employee

Hello @GMeta.1,

I'm not sure to understand it fully, there's already the name of the custom container in the properties :

LouisB_0-1724757958403.png

 

Best Regards,

Louis BOUDO
ST Software Developer | TouchGFX

View solution in original post

2 REPLIES 2
LouisB
ST Employee

Hello @GMeta.1,

I'm not sure to understand it fully, there's already the name of the custom container in the properties :

LouisB_0-1724757958403.png

 

Best Regards,

Louis BOUDO
ST Software Developer | TouchGFX

Hi

OK maybe that was added recently. I am using version 4.19.1 and it doesn't have that:

touchgfx1.png