2022-07-10 07:20 AM
2022-07-10 09:50 AM
Normal place of instal isnt in ProgramFiles then your isuue must be other type. Try show error...
2022-07-10 11:14 PM
But I I installed in another place due to some reasons.
The Build tries to build under Programs files and generates and an error the the files are not there..
2022-07-11 09:24 AM
show error
2022-07-15 02:16 AM
Hello ECrom.2,
TouchGFX Designer could be installed anywhere on your computer. HOWEVER you must install STM32CubeProgrammer to the default path which is "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer" because this is where TouchGFX Designer will look for when you run on target.
/Osman
2022-07-16 08:29 PM
Thanks
There should be a configuration param for this
Eli